Unable to get PCIE driver logs in WIndows 10 IoT in NXP IMX8M Plus EVK board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to get PCIE driver logs in WIndows 10 IoT in NXP IMX8M Plus EVK board

443件の閲覧回数
Ben10
Contributor II

We are trying to get the log messages from the PCIE driver in windows 10 IoT in the NXP IMX8M Plus EVK board, but we are not able to get any logs. We have built the firmware in the debug mode and we have also enabled debug in the PCIE driver, but even after that we are not getting the debug messages from the PCIE driver. We are using the latest release of the Windows 10 IoT BSP (W21H2-1-5-0).

So, what should we do to get the PCIE driver log messages?

I have also attached the UEFI log for your reference.

0 件の賞賛
1 返信

422件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The buildme64.sh script bundled in BSP also copies flash.binand uefi.fit into <BSP_DIR> /
imx-windows-iot/components/Arm64BootFirmware/<board_name>. It allows rebuilding only UEFI
or U-Boot.

Use -b MX8M_PLUS_EVK or -b 8Mp to select i.MX 8M Plus EVK

in uboot can not get PCI log messages, sorry this is a enhancement for 1.6 v.

 

Regards

 

0 件の賞賛