Unable to enter keystroke at login console after booting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to enter keystroke at login console after booting

254 Views
pawan4749
Contributor I

I'm not able to login to imx 6 panel after booting successfully. Panel stuck at login prompt and not accepting any keyboard stroke. Tried with multiple serial cables and on different consoles.

U-Boot 2020.04 (Jan 05)

CPU: i.MX6DL rev1.4 at 792 MHz
Reset cause: POR
Board: ADT-AIOBT 200-01939v4a
I2C: ready
DRAM: 256 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
In: serial
Out: serial
Err: serial
facmod value is 1!
Net: Board Net Initialization Failed
No ethernet found.
Normal Boot
Hit any key to stop autoboot: 0
resetting ...


U-Boot 2020.04 (Jan 05 2022)

CPU: i.MX6DL rev1.4 at 792 MHz
Reset cause: WDOG
Board: ADT-AIOBT 200-01939v4a
I2C: ready
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
In: serial
Out: serial
Err: serial
facmod value is 1!
Net: Board Net Initialization Failed
No ethernet found.
Normal Boot
Hit any key to stop autoboot: 0
** Invalid partition 3 **
uEnv not found in mmcpart3, checking mmcpart1
67 bytes read in 155 ms (0 Bytes/s)
uEnv found in mmcpart 1!
Booting from mmc ...
w=zZbB1ZDVhY2UxMjUwYjI0OTFkNAo=980
384 bytes read in 171 ms (2 KiB/s)
18112886 bytes read in 628 ms (27.5 MiB/s)
## Loading kernel from FIT Image at 12000000 ...
Using 'conf@hon-adt-aio-200-01939v4a.dtb' configuration
Trying 'kernel@1' kernel subimage
Description: Linux kernel
Type: Kernel Image
Compression: uncompressed
Data Start: 0x120000ec
Data Size: 7961472 Bytes = 7.6 MiB
Architecture: ARM
OS: Linux
Load Address: 0x10008000
Entry Point: 0x10008000
Hash algo: sha256
Hash value: e2d339f3bb707e4623d08cbcf3750edc82c94d992d3957f0b6b5a067ab935979
Verifying Hash Integrity ... sha256+ OK
## Loading ramdisk from FIT Image at 12000000 ...
Using 'conf@hon-adt-aio-200-01939v4a.dtb' configuration
Trying 'ramdisk@1' ramdisk subimage
Description: initramfs-ostree-image
Type: RAMDisk Image
Compression: uncompressed
Data Start: 0x1289a168
Data Size: 8701725 Bytes = 8.3 MiB
Architecture: ARM
OS: Linux
Load Address: unavailable
Entry Point: unavailable
Hash algo: sha256
Hash value: ac0bdc013a3eeceb1dfef104018a61f654f195550b1ef9ffce1b785e83c56034
Verifying Hash Integrity ... sha256+ OK
## Loading fdt from FIT Image at 12000000 ...
Using 'conf@hon-adt-aio-200-01939v4a.dtb' configuration
Trying 'fdt@hon-adt-aio-200-01939v4a.dtb' fdt subimage
Description: Flattened Device Tree blob
Type: Flat Device Tree
Compression: uncompressed
Data Start: 0x12834598
Data Size: 48205 Bytes = 47.1 KiB
Architecture: ARM
Hash algo: sha256
Hash value: fdfb63364de8d622939fc84081444402a165978df7e0bb95dc3690c5ff67b6c0
Verifying Hash Integrity ... sha256+ OK
Booting using the fdt blob at 0x12834598
Loading Kernel Image
Loading Device Tree to 2ef73000, end 2ef81c4c ... OK

Starting kernel ...


Starting kernel ...

[ 0.607148] imx6dl-pinctrl 20e0000.iomuxc: pin MX6DL_PAD_DISP0_DAT11 already requested by 1-0058; cannot claim for 1-0055
[ 0.618146] imx6dl-pinctrl 20e0000.iomuxc: pin-47 (1-0055) status -22
[ 0.624608] imx6dl-pinctrl 20e0000.iomuxc: could not request pin 47 (MX6DL_PAD_DISP0_DAT11) from group ctpgrp on device 20e0000.iomuxc
[ 0.636793] st1633-ts 1-0055: Error applying setting, reverse things back
[ 0.891667] debugfs: Directory '202c000.ssi' with parent 'tlv320aic3120-audio' already present!
[ 0.902175] debugfs: Directory '2028000.ssi' with parent 'imx-audio-lte' already present!
[ 1.237034] imx6q-pcie 1ffc000.pcie: failed to initialize host
[ 1.242879] imx6q-pcie 1ffc000.pcie: unable to add pcie port.
/sbin/init[1]: Starting OSTree initrd script
/sbin/init[1]: mounting FS: proc /proc
/sbin/init[1]: mounting FS: sysfs /sys
/sbin/init[1]: mounting FS: devtmpfs /dev
/sbin/init[1]: /dev (devtmpfs) already mounted
/sbin/init[1]: mounting FS: devpts /dev/pts
/sbin/init[1]: mounting FS: tmpfs /dev/shm
/sbin/init[1]: mounting FS: tmpfs /tmp
/sbin/init[1]: mounting FS: tmpfs /run
checking root partition filesystem
e2fsck 1.45.6 (20-Mar-2020)
ROOTFS_A: recovering journal
Setting free inodes count to 918704 (was 918706)
Setting free blocks count to 608627 (was 609048)
ROOTFS_A: clean, 29296/948000 files, 357773/966400 blocks
4800+0 records in
4800+0 records out
/sbin/init[1]: Moving /dev to new rootfs
/sbin/init[1]: Moving /proc to new rootfs
/sbin/init[1]: Switching to new rootfs
/sbin/init[1]: Launching target init
[ 6.643525] ERROR: v4l2 capture: slave not found!
▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒
GRIP Quicksilver 03.1362.0 GRIP-48A2E6441F5E ttymxc0

GRIP-48A2E6441F5E login:

[ 25.981518] spi-nor spi3.0: unrecognized JEDEC id bytes: ff ff ff ff ff ff
[ 28.853138] spi-nor spi3.0: unrecognized JEDEC id bytes: ff ff ff ff ff ff

0 Kudos
0 Replies