Unable to create system.img for android lollipop

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to create system.img for android lollipop

ソリューションへジャンプ
2,530件の閲覧回数
kishorepoojari
Contributor III

Hello All ,

  When I building android(Lollipop 5.0.0.1) for imx6slevk board , system.img is not able to generate.

Following error is obtained:

Install system fs image: out/target/product/evk_6sl/system_sparse.img

out/target/product/evk_6sl/system_sparse.img+out/target/product/evk_6sl/obj/PACKAGING/recovery_patch_intermediates/recovery_from_boot.p maxsize=481738752 blocksize=4224 total=403801046 reserve=4866048

if [ true = true ]; then \

        simg2img out/target/product/evk_6sl/system_sparse.img out/target/product/evk_6sl/system.img; \

        fi

/bin/bash: line 1: simg2img: command not found

make: *** [out/target/product/evk_6sl/system_sparse.img] Error 127

make: *** Deleting file `out/target/product/evk_6sl/system_sparse.img'

I have installed all package listed in the Android User guide as well as Establishing a Build Environment | Android Open Source Project

still any package are missing...?

please help me sort out this issue...

Regards,

Kishore P

ラベル(3)
タグ(1)
0 件の賞賛
返信
1 解決策
1,727件の閲覧回数
kishorepoojari
Contributor III

Hello Gusarambula ,

   I have give the full path with the "simg2img" to solve the issue.

if [ true = true ]; then \

        /home/test/Android_Source/out/host/linux-x86/bin/simg2img out/target/product/evk_6sl/system_sparse.img  out/target/product/evk_6sl/system.img; \

        fi

Regards,

Kishore P

元の投稿で解決策を見る

2 返答(返信)
1,727件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kishore Poojari,

Are you still experiencing issues building Android? Have you followed the Android User’s Guide step by step? If so, did you receive any error message when downloading or patching the source code?

0 件の賞賛
返信
1,728件の閲覧回数
kishorepoojari
Contributor III

Hello Gusarambula ,

   I have give the full path with the "simg2img" to solve the issue.

if [ true = true ]; then \

        /home/test/Android_Source/out/host/linux-x86/bin/simg2img out/target/product/evk_6sl/system_sparse.img  out/target/product/evk_6sl/system.img; \

        fi

Regards,

Kishore P