Unable to connect the imx8mp solidrun board with another board over bluetooth

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to connect the imx8mp solidrun board with another board over bluetooth

471件の閲覧回数
manoj1
Contributor I

Hi,

Am using two imx8mp solidrun boards to connect over Bluetooth using bluetoothctl command tool.

But am getting the below log message.
failed to connect: org.bluez.error.notavailable br-connection-profile-unavailable.

Please let me know the procedure of connection between boards.

Note: if I use mobile device to connect over bluetooth it is connected by sharing the passkey.

Please find the below screenshot and /etc/systemd/system/dbus-org.bluez.service file configurations.

manoj1_0-1713530254691.png

[Unit]
Description=Bluetooth service
Documentation=man:bluetoothd(8)
ConditionPathIsDirectory=/sys/class/bluetooth

[Service]
Type=dbus
BusName=org.bluez
ExecStart=/usr/lib/bluetooth/bluetoothd
NotifyAccess=main
#WatchdogSec=10
Restart=on-failure
CapabilityBoundingSet=CAP_NET_ADMIN CAP_NET_BIND_SERVICE
LimitNPROC=1
ProtectHome=true
ProtectSystem=full

[Install]
WantedBy=bluetooth.target
Alias=dbus-org.bluez.service

 

Regards

0 件の賞賛
返信
2 返答(返信)

436件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Make sure that you are using the latest bsp since all this steps works in bluettooth mode, I guess someone from @nitrogen can help you.

Regards

0 件の賞賛
返信

432件の閲覧回数
manoj1
Contributor I

Yes, Am using latest bsp version only.

Please let me know the steps if anything I missed. 

Regards

0 件の賞賛
返信