Unable to connect the JTAG to i.MX6 Quad processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to connect the JTAG to i.MX6 Quad processor

1,124件の閲覧回数
muralikrishna
Contributor I

We are using i.MX6 Quad Processor in our design.  The boards are fabricated with i.MX6 processor. In the new boards we are unable to connect the J-Link JTAG (Segger). When we connect J-link JTAG, it is dipalying as message that Device is not connected at all" and it is not diplaying device id also.

For new processors is we need to program first anything before JTAG communication. Kindly clarify.

ラベル(1)
0 件の賞賛
返信
1 返信

574件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please check Your design regarding Design Checklist recommendations in Chapter 2

(Design Checklist) of IMX6DQ6SDLHDG : Hardware Development Guide for i.MX 6Quad,

6Dual, 6DualLite, 6Solo Families

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Please pay attention on Table 2-5 (JTAG recommendations).

Also, the following may be useful :

Re: Debugging U-boot on iMX6

Re: J-Link and iMX6


Have a great day,
Yuri.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信