But as per datasheet of IMX6ULL the processor have tamper detection feature.
Hello,
According to i.MX 6ULL Migration Guide:
The advanced security features that are mainly used by the POS applications (including CAAM/BEE/DryICE)
are removed.
https://www.nxp.com/docs/en/application-note/AN5350.pdf
The tamper pins cannot be used in i.MX 6ULL, because of factory pre-programmed state of the
corresponding fuses.
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------