Unable to caliberate LPDDR3 with IMX7D

cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to caliberate LPDDR3 with IMX7D

267 Views
flabyjacob
Contributor III

Hello There,

I am working on custom IMX7D board based on imx7 dual sabre board. I am trying to use the same uboot code from reference design, but unlike the reference board, in my design I have only single DDR3 of 4Gb. So are there any changes which I should make in the uboot or will it take care itself?

Thanks in advance.

Labels (1)
Tags (3)
0 Kudos
1 Reply

159 Views
Yuri
NXP TechSupport
NXP TechSupport

Hello,

 

  Use Chapter 3 (Porting U-Boot) of  i.MX_Porting_Guide.pdf in Linux documentation.

https://www.nxp.com/webapp/Download?colCode=imx-yocto-L4.14.98_2.0.0_ga 

  The following tools may be helpful:

i.MX6/7 DDR Stress Test Tool V3.00 

https://community.nxp.com/docs/DOC-152468  

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos