Unable to boot from eMMC in imx8mm

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unable to boot from eMMC in imx8mm

758 次查看
BhavinJoisar
Contributor I

Greetings,

I am building linux OS for custom board and imx8mm, I am able to boot my custom board from SD card which is connected at usdhc2 but I am unable to boot from eMMC which is at usdhc3. I am getting he following error message.

U-Boot SPL 2020.04-v2020.04_5.4.24_2.1.0_dunfell+ga85da91ab8 (Mar 01 2023 - 07:33:33 +0000)
power_bd71837_init
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from MMC2

U-Boot 2020.04-v2020.04_5.4.24_2.1.0_dunfell+ga85da91ab8 (Mar 01 2023 - 07:33:33 +0000)

CPU: i.MX8MMQ rev1.0 1600 MHz (running at 1200 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 29C
Reset cause: POR
Model: Trucrux TRUX-MX8M-MINI
DRAM: 512 MiB
MMC: FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... *** Warning - bad CRC, using default environment

In: serial
Out: serial
Err: serial

BuildInfo:
- ATF
- U-Boot 2020.04-v2020.04_5.4.24_2.1.0_dunfell+ga85da91ab8

flash target is MMC:2
Net: Could not get PHY for FEC0: addr 0
Could not get PHY for FEC0: addr 0
No ethernet found.

Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
Card did not respond to voltage select!
MMC Device 0 not found
no mmc device at slot 0
Bad Linux ARM64 Image magic!
u-boot=>

 

Below is the node in imx8mm-board.dtsi

pinctrl_usdhc3: usdhc3grp {
fsl,pins = <
MX8MM_IOMUXC_NAND_WE_B_USDHC3_CLK 0x190
MX8MM_IOMUXC_NAND_WP_B_USDHC3_CMD 0x1d0
MX8MM_IOMUXC_NAND_DATA04_USDHC3_DATA0 0x1d0
MX8MM_IOMUXC_NAND_DATA05_USDHC3_DATA1 0x1d0
MX8MM_IOMUXC_NAND_DATA06_USDHC3_DATA2 0x1d0
MX8MM_IOMUXC_NAND_DATA07_USDHC3_DATA3 0x1d0
MX8MM_IOMUXC_NAND_RE_B_USDHC3_DATA4 0x1d0
MX8MM_IOMUXC_NAND_CE2_B_USDHC3_DATA5 0x1d0
MX8MM_IOMUXC_NAND_CE3_B_USDHC3_DATA6 0x1d0
MX8MM_IOMUXC_NAND_CLE_USDHC3_DATA7 0x1d0
MX8MM_IOMUXC_NAND_CE1_B_USDHC3_STROBE 0x190
>;
};

pinctrl_usdhc3_100mhz: usdhc3grp100mhz {
fsl,pins = <
MX8MM_IOMUXC_NAND_WE_B_USDHC3_CLK 0x194
MX8MM_IOMUXC_NAND_WP_B_USDHC3_CMD 0x1d4
MX8MM_IOMUXC_NAND_DATA04_USDHC3_DATA0 0x1d4
MX8MM_IOMUXC_NAND_DATA05_USDHC3_DATA1 0x1d4
MX8MM_IOMUXC_NAND_DATA06_USDHC3_DATA2 0x1d4
MX8MM_IOMUXC_NAND_DATA07_USDHC3_DATA3 0x1d4
MX8MM_IOMUXC_NAND_RE_B_USDHC3_DATA4 0x1d4
MX8MM_IOMUXC_NAND_CE2_B_USDHC3_DATA5 0x1d4
MX8MM_IOMUXC_NAND_CE3_B_USDHC3_DATA6 0x1d4
MX8MM_IOMUXC_NAND_CLE_USDHC3_DATA7 0x1d4
MX8MM_IOMUXC_NAND_CE1_B_USDHC3_STROBE 0x194
>;
};

pinctrl_usdhc3_200mhz: usdhc3grp200mhz {
fsl,pins = <
MX8MM_IOMUXC_NAND_WE_B_USDHC3_CLK 0x196
MX8MM_IOMUXC_NAND_WP_B_USDHC3_CMD 0x1d6
MX8MM_IOMUXC_NAND_DATA04_USDHC3_DATA0 0x1d6
MX8MM_IOMUXC_NAND_DATA05_USDHC3_DATA1 0x1d6
MX8MM_IOMUXC_NAND_DATA06_USDHC3_DATA2 0x1d6
MX8MM_IOMUXC_NAND_DATA07_USDHC3_DATA3 0x1d6
MX8MM_IOMUXC_NAND_RE_B_USDHC3_DATA4 0x1d6
MX8MM_IOMUXC_NAND_CE2_B_USDHC3_DATA5 0x1d6
MX8MM_IOMUXC_NAND_CE3_B_USDHC3_DATA6 0x1d6
MX8MM_IOMUXC_NAND_CLE_USDHC3_DATA7 0x1d6
MX8MM_IOMUXC_NAND_CE1_B_USDHC3_STROBE 0x196
>;
};

 

/* EMMC */
&usdhc3 {
pinctrl-names = "default", "state_100mhz", "state_200mhz";
pinctrl-0 = <&pinctrl_usdhc3>;
pinctrl-1 = <&pinctrl_usdhc3_100mhz>;
pinctrl-2 = <&pinctrl_usdhc3_200mhz>;
bus-width = <8>;
non-removable;
status = "okay";
};

 

It would be great if anyone can help.

0 项奖励
回复
1 回复

730 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @BhavinJoisar 

The clock in spl.c (uboot-imx/board/freescale/imx8mm_evk/spl.c) doesn't enable for uSDHC3 for DDR4 board.

You can try to modify like:  for (i = 0; i < 2; i++)

 

Best regards

Harvey

0 项奖励
回复