Unable to boot from SPI-NOR on imx6q-sdb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to boot from SPI-NOR on imx6q-sdb

1,937 Views
linhsun
Contributor III

Dear all

   My board is imx6q-sdb broad, I setting boot mode to SPI mode, after weld a spi-flash chip (U14, R643, R646, R149 C83, can see figure 1),  last flash an u-boot.bin to NOR Flash (use mfgtool), but can not load bootloader from SPI(always into download mode), please get me several suggest(is something missing?), thank.

NOTE:I believe SPI NOR has code(use mfgtool flash u-boot to NOR is success), will be into bootloader

My config information:

 SBMR1 ---> 0x18000030 

 BOOT_CFG1[7:4] --> 0011

 BOOT_CFG4[5:4] --> 01 - ECSPIx_SS1

 BOOT_CFG4[3]    --> 1 - 3-bytes (24-bit)

 BOOT_CFG4[2:0] --> 000 - ECSPI-1

figure 1

pastedImage_2.png

figure 2

pastedImage_19.png

Labels (3)
0 Kudos
Reply
2 Replies

1,730 Views
igorpadykov
NXP Employee
NXP Employee

Hi Lin

according to Table 14. Known issues and workarounds for i.MX 6 SABRE-SD

attached Linux Release Notes:

SPI NOR boot is not supported by the SABRE-SD board.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,730 Views
linhsun
Contributor III

Dear igor

   Thank very much. 

0 Kudos
Reply