Dear all
My board is imx6q-sdb broad, I setting boot mode to SPI mode, after weld a spi-flash chip (U14, R643, R646, R149 C83, can see figure 1), last flash an u-boot.bin to NOR Flash (use mfgtool), but can not load bootloader from SPI(always into download mode), please get me several suggest(is something missing?), thank.
NOTE:I believe SPI NOR has code(use mfgtool flash u-boot to NOR is success), will be into bootloader
My config information:
SBMR1 ---> 0x18000030
BOOT_CFG1[7:4] --> 0011
BOOT_CFG4[5:4] --> 01 - ECSPIx_SS1
BOOT_CFG4[3] --> 1 - 3-bytes (24-bit)
BOOT_CFG4[2:0] --> 000 - ECSPI-1
figure 1
figure 2
Hi Lin
according to Table 14. Known issues and workarounds for i.MX 6 SABRE-SD
attached Linux Release Notes:
SPI NOR boot is not supported by the SABRE-SD board.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear igor
Thank very much.