Unable to boot Windows IOT Core on IMX6ULL EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to boot Windows IOT Core on IMX6ULL EVK

1,520件の閲覧回数
lokeshvenkatara
Contributor II

Hello Experts,

I am trying to boot imx6ull board using pre-built windows IOT core image downloaded from the NXP website.

However I am getting following errors while booting from microSD card.

I have tried both W1809_1_1_0 Prebuilt image for MCIMX6ULL-EVK board and W1806_1_0_1_MCIMX6ULL-EVK Image and getting the same error from both the images.

pastedImage_1.png

Note: I am using sandisk microSD ultra speed class 10 card recommended by the microsoft. I assume sd card has not an issue, since Raspberry pi is booting from the same sd card when I load windows IOT core ffu.

Kindly let us know what we are missing and what is causing the above issue.

         ##

ラベル(3)
0 件の賞賛
3 返答(返信)

1,354件の閲覧回数
petr_kovar
NXP Employee
NXP Employee

Hi Lokesh,

From image with console output it looks like it should boot up even with this SD card error. Is the board really unable to boot up? When you connect display are you able to see windows dashboard? Or are you able to connect to board via Windows Device Portal? (Windows Device Portal - Windows IoT | Microsoft Docs )

Petr

0 件の賞賛

1,353件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hi,

to avoid the "Write Protected" report is necessary to add following into *.dsc file (new lines marked as bold):

giMXPlatformTokenSpaceGuid.PcdSdhc2Enable|TRUE
giMXPlatformTokenSpaceGuid.PcdSdhc2CardDetectSignal|0xFF00
giMXPlatformTokenSpaceGuid.PcdSdhc2WriteProtectSignal|0xFF00

EVK_iMX6ULL_512MB.dsc is located here:

imx-edk2-platforms/Platform/NXP/EVK_iMX6ULL_512MB/EVK_iMX6ULL_512MB.dsc

UEFI image (uefi.fit) must be updated after this step. You can copy it into UEFI partiton on sd card. For ffu image is necessary to have the updated version here:

imx-iotcore\build\board\EVK_iMX6ULL_512MB\Package\BootFirmware\uefi.fit

bets regards

Vojtech Filip

1,353件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Lokesh,

Is this error shown while booting the board or are you unable to load the image to the SD card?

I would recommend using the latest images from the W1809 release as it fixes a boot problem with the i.MX6ULL. If the problem occurs when writing to the SD card please make sure that you are following the steps on the User’s Guide available on the link below (you may need to login to download this document)

https://www.nxp.com/webapp/Download?colCode=W1809_1_1_0_i.MX_Win10_Users_Guide&appType=license

The newer release images can be downloaded from the following page:

https://www.nxp.com/design/software/embedded-software/windows-10-iot-core-for-i-mx-applications-proc...

I hope this helps!

Regards,

0 件の賞賛