Unable to boot LF_v6.1.36-2.1.0_images_IMX93EVK image using microSD card on i.MX 93 EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to boot LF_v6.1.36-2.1.0_images_IMX93EVK image using microSD card on i.MX 93 EVK

172 Views
sandeep_arm
Contributor I

Hi there,

I'm trying to use the pre-built imx-image-full-imx93evk.wic image from the LF_v6.1.36-2.1.0_images_IMX93EVK release. However, I see no serial output after flashing it to a microSD card and using the microSD card on the i.MX 93 EVK board.

 imx-image-full-imx93evk.wic images from the LF_v6.1.22-2.0.0_images_IMX93EVK and LF_v6.1.1_1.0.0_images_IMX93EVK releases do work.

 

Does anyone have suggestions on what to try to resolve this?

0 Kudos
2 Replies

147 Views
sandeep_arm
Contributor I

Hi @Chavira,

 

Thank you for the prompt and clear answer. In the short term, I'll switch to using the 6.1.22 release, and look into getting an EVK board with the A1 silicon.

 

0 Kudos

159 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @sandeep_arm!
Thank you for contacting NXP Support!

You have the iMX93 Evk with Silicon A0 (pre-production).

That chip only supports the release 6.1.22 and 6.1.1.

The A1 Silicon is compatible with releases 6.1.36 and 6.1.55 and the next releases.

Sorry for the mistake!

Best Regards!
Chavira