Unable to access the git repo repo init -u git://git.freescale.com/imx/linux-2.6-imx.git -b imx-4.1.15-1.0.0_ga

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to access the git repo repo init -u git://git.freescale.com/imx/linux-2.6-imx.git -b imx-4.1.15-1.0.0_ga

7,984 Views
prashs
Contributor I

Hi,


I am trying to check out the yocto recipes for the Variscite platform

I am getting this error message when I try to do a repo init on the git URL

$ repo init -u git://git.freescale.com/imx/linux-2.6-imx.git -b imx-4.1.15-1.0.0_ga

fatal: unable to connect to git.freescale.com:
git.freescale.com[0: 192.88.156.202]: errno=Connection refused

fatal: unable to connect to git.freescale.com:
git.freescale.com[0: 192.88.156.202]: errno=Connection refused

fatal: cannot obtain manifest git://git.freescale.com/imx/linux-2.6-imx.git

The IP address  192.88.156.202 is not reachable. But I am able to open the Git HUB page using the browser

git://git.freescale.com/imx/fsl-arm-yocto-bsp.git

Thanks !

Tags (4)
0 Kudos
Reply
5 Replies

5,164 Views
vijayaragavansr
Contributor II

Hi All,

am able to download the content from git now.

i built core-image-base and set root password and mounted over NFS and things are working as expected.

but when i execute the command poweroff,reboot,shutdown is asking for super user,

below is the message from terminal

root@hello:~# poweroff
poweroff: must be superuser.
root@hello:~# reboot
reboot: must be superuser.
root@hello:~# shutdown -r now
shutdown: warning: cannot open /var/run/shutdown.pid
shutdown: /dev/initctl: Permission denied
init: must be superuser.
root@hello:~# cat /etc/passwd

root:x:0:0:root:/home/root:/bin/sh
daemon:x:1:1:daemon:/usr/sbin:/bin/sh
bin:x:2:2:bin:/bin:/bin/sh
sys:x:3:3:sys:/dev:/bin/sh
sync:x:4:65534:sync:/bin:/bin/sync
games:x:5:60:games:/usr/games:/bin/sh
man:x:6:12:man:/var/cache/man:/bin/sh
lp:x:7:7:lp:/var/spool/lpd:/bin/sh
mail:x:8:8:mail:/var/mail:/bin/sh
news:x:9:9:news:/var/spool/news:/bin/sh
uucp:x:10:10:uucp:/var/spool/uucp:/bin/sh
proxy:x:13:13:proxy:/bin:/bin/sh
www-data:x:33:33:www-data:/var/www:/bin/sh
backup:x:34:34:backup:/var/backups:/bin/sh
list:x:38:38:Mailing List Manager:/var/list:/bin/sh
irc:x:39:39:ircd:/var/run/ircd:/bin/sh
gnats:x:41:41:Gnats Bug-Reporting System (admin):/var/lib/gnats:/bin/sh
nobody:x:65534:65534:nobody:/nonexistent:/bin/sh
rpc:x:999:999::/:/bin/false
avahi:x:998:998::/var/run/avahi-daemon:/bin/false
sshd:x:997:997::/var/run/sshd:/bin/false
messagebus:x:996:995::/var/lib/dbus:/bin/false
rpcuser:x:995:994::/var/lib/nfs:/bin/false
pulse:x:994:1001::/var/run/pulse:/bin/false

root@hello:~# cat /etc/shadow
root:$6$kTvdT/eRFpQ/ZDeA$tBghQG.52TsnHOxaanBo.MtKbKowBwaZtGKBdNPoW.w66xexzRcPbtHFyDO.yP04L.tnsMkcGgGSmpx3rAvMC/:17081:0:99999:7:::
daemon:*:17081:0:99999:7:::
bin:*:17081:0:99999:7:::
sys:*:17081:0:99999:7:::
sync:*:17081:0:99999:7:::
games:*:17081:0:99999:7:::
man:*:17081:0:99999:7:::
lp:*:17081:0:99999:7:::
mail:*:17081:0:99999:7:::
news:*:17081:0:99999:7:::
uucp:*:17081:0:99999:7:::
proxy:*:17081:0:99999:7:::
www-data:*:17081:0:99999:7:::
backup:*:17081:0:99999:7:::
list:*:17081:0:99999:7:::
irc:*:17081:0:99999:7:::
gnats:*:17081:0:99999:7:::
nobody:*:17081:0:99999:7:::
rpc:!:17081::::::
avahi:!:17081::::::
sshd:!:17081::::::
messagebus:!:17081::::::
rpcuser:!:17081::::::
pulse:!:17081::::::

root@hello:~# cat /etc/sudoers
## sudoers file.
##
## This file MUST be edited with the 'visudo' command as root.
## Failure to use 'visudo' may result in syntax or file permission errors
## that prevent sudo from running.
##
## See the sudoers man page for the details on how to write a sudoers file.
##

##
## Host alias specification
##
## Groups of machines. These may include host names (optionally with wildcards),
## IP addresses, network numbers or netgroups.
# Host_Alias WEBSERVERS = www1, www2, www3

##
## User alias specification
##
## Groups of users. These may consist of user names, uids, Unix groups,
## or netgroups.
# User_Alias ADMINS = millert, dowdy, mikef

##
## Cmnd alias specification
##
## Groups of commands. Often used to group related commands together.
# Cmnd_Alias PROCESSES = /usr/bin/nice, /bin/kill, /usr/bin/renice, \
# /usr/bin/pkill, /usr/bin/top
# Cmnd_Alias REBOOT = /sbin/halt, /sbin/reboot, /sbin/poweroff

##
## Defaults specification
##
## You may wish to keep some of the following environment variables
## when running commands via sudo.
##
## Locale settings
# Defaults env_keep += "LANG LANGUAGE LINGUAS LC_* _XKB_CHARSET"
##
## Run X applications through sudo; HOME is used to find the
## .Xauthority file. Note that other programs use HOME to find
## configuration files and this may lead to privilege escalation!
# Defaults env_keep += "HOME"
##
## X11 resource path settings
# Defaults env_keep += "XAPPLRESDIR XFILESEARCHPATH XUSERFILESEARCHPATH"
##
## Desktop path settings
# Defaults env_keep += "QTDIR KDEDIR"
##
## Allow sudo-run commands to inherit the callers' ConsoleKit session
# Defaults env_keep += "XDG_SESSION_COOKIE"
##
## Uncomment to enable special input methods. Care should be taken as
## this may allow users to subvert the command being run via sudo.
# Defaults env_keep += "XMODIFIERS GTK_IM_MODULE QT_IM_MODULE QT_IM_SWITCHER"
##
## Uncomment to use a hard-coded PATH instead of the user's to find commands
# Defaults secure_path="/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin"
##
## Uncomment to send mail if the user does not enter the correct password.
# Defaults mail_badpass
##
## Uncomment to enable logging of a command's output, except for
## sudoreplay and reboot. Use sudoreplay to play back logged sessions.
# Defaults log_output
# Defaults!/usr/bin/sudoreplay !log_output
# Defaults!/usr/local/bin/sudoreplay !log_output
# Defaults!REBOOT !log_output

##
## Runas alias specification
##

##
## User privilege specification
##
root ALL=(ALL) ALL

## Uncomment to allow members of group wheel to execute any command
# %wheel ALL=(ALL) ALL

## Same thing without a password
# %wheel ALL=(ALL) NOPASSWD: ALL

## Uncomment to allow members of group sudo to execute any command
# %sudo ALL=(ALL) ALL

## Uncomment to allow any user to run sudo if they know the password
## of the user they are running the command as (root by default).
# Defaults targetpw # Ask for the password of the target user
# ALL ALL=(ALL) ALL # WARNING: only use this together with 'Defaults targetpw'

## Read drop-in files from /etc/sudoers.d
## (the '#' here does not indicate a comment)
#includedir /etc/sudoers.d

i tried all images like core-image-base,fsl-gui-image,etc...

and this is the content of local.conf 

MACHINE ??= 'imx6ulevk'
DISTRO ?= 'fsl-imx-x11'
PACKAGE_CLASSES ?= "package_rpm"
#EXTRA_IMAGE_FEATURES = "debug-tweaks"
EXTRA_IMAGE_FEATURES = "ssh-server-openssh"
INHERIT += "extrausers"
EXTRA_USERS_PARAMS = "usermod -P hello root;"
USER_CLASSES ?= "buildstats image-mklibs"
PATCHRESOLVE = "noop"
BB_DISKMON_DIRS = "\
STOPTASKS,${TMPDIR},1G,100K \
STOPTASKS,${DL_DIR},1G,100K \
STOPTASKS,${SSTATE_DIR},1G,100K \
STOPTASKS,/tmp,100M,100K \
ABORT,${TMPDIR},100M,1K \
ABORT,${DL_DIR},100M,1K \
ABORT,${SSTATE_DIR},100M,1K \
ABORT,/tmp,10M,1K"
#PACKAGECONFIG_append_pn-qemu-native = " sdl"
#PACKAGECONFIG_append_pn-nativesdk-qemu = " sdl"
BUILD_LDFLAGS_prepend_pn-qemu-native = "-Wl,-rpath-link,/lib/x86_64-linux-gnu "
ASSUME_PROVIDED += "libsdl-native"
CONF_VERSION = "1"

DL_DIR ?= "${BSPDIR}/downloads/"
ACCEPT_FSL_EULA = "1"

am struck here...

0 Kudos
Reply

5,164 Views
b36401
NXP Employee
NXP Employee

It should be network (possibly firewall) issue.
Please note that git default port is 9418.
I mean when you access git.freescale.com with browser it goes to port 80 but repo goes to port 9418.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

5,164 Views
prashs
Contributor I

Hi,

The issue appears to have been fixed now.

I am able to do a repo init and sync successfully.

$ repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1.15-1.0.0_ga

$ repo sync

Please mark this issue as fixed.

Thanks,

Prashanth

0 Kudos
Reply

5,164 Views
joanxie
NXP TechSupport
NXP TechSupport

could you access any internet from your host? sometimes proxy cause this issue.

and try to use git clone to replace repo, likt "git clone git://"

0 Kudos
Reply

5,164 Views
vijayaragavansr
Contributor II

I too have the same issue... struck exact at this point.

0 Kudos
Reply