Unable to Enable Dual Ethernet Functionality on i.MX8QXP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to Enable Dual Ethernet Functionality on i.MX8QXP

2,254 Views
adnan_dst
Contributor III

Hello,

I am working on an i.MX8QXP with a custom carrier board that includes two Ethernet interfaces (KSZ9031RNXVB-TRVAO).

When configuring a single Ethernet interface (ethphy0), the dmesg log shows the link is up at 10 Mbps half-duplex with flow control off, and the assigned IP is in the 169...* range. However, enabling autonegotiation allows eth0 to obtain an IP address and successfully handle tasks like pinging and file transfers.

The issue arises when enabling both Ethernet interfaces in the device tree. The logs indicate a failure to connect to the PHY for both eth0 and eth1. Additionally, the mdio info command in U-Boot reports: No MDIO bus found.

I have attached the relevant device tree files and schematics. Please advise on the steps required to get both Ethernet interfaces operational.


Thanks.

0 Kudos
Reply
3 Replies

2,252 Views
adnan_dst
Contributor III
We are using a single MDIO interface to connect two Ethernet PHYs. Is it acceptable to use a single MDIO interface in this setup, or are there any changes required to ensure proper functionality?
0 Kudos
Reply

2,221 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

Could you share your <board>.c from u-boot?

Regards

0 Kudos
Reply

2,198 Views
adnan_dst
Contributor III

Hello,

Below is my board.c file from u-boot source.

Thanks!

0 Kudos
Reply