Ubuntu-desktop is needed for GUI?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ubuntu-desktop is needed for GUI?

2,769 Views
ajayvenkatakris
Contributor II

Hi, 

   I am currently running my IMX6 Sabre auto with the full Ubuntu 14.04 rootfs. Although it is working properly through the serial connection, I am not getting the GUI through HDMI connection. Is the ubuntu-desktop unity required for the GUI to show?

0 Kudos
Reply
3 Replies

2,564 Views
art
NXP Employee
NXP Employee

Also, refer to the attached documents. Hope it will be helpful.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,564 Views
jimmychan
NXP TechSupport
NXP TechSupport

https://community.nxp.com/docs/DOC-330147 

Hope this information help you.

0 Kudos
Reply

2,564 Views
ajayvenkatakris
Contributor II

Hi,

   I have installed ubuntu-desktop but I am getting an error saying that the system is running on low graphics mode. How do I solve this error?

0 Kudos
Reply