Ubuntu 12.04 and L2.6.35_11.09.01_ER_source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ubuntu 12.04 and L2.6.35_11.09.01_ER_source

1,230 Views
ShaneKaiser
Contributor II

Hello Everyone,


Has anyone been able to successfully build L2.6.35_11.09.01_ER_source for i.MX53 QSB on Ubuntu 12.04?


I tried and I am getting errors.


The current error is:

collect2: ld returned 1 exit status
make: *** [mconf] Error 1
error: Bad exit status from /home/imx53/11.09.01/ltib/tmp/rpm-tmp.40833 (%build)
RPM build errors:
    Bad exit status from /home/imx53/11.09.01/ltib/tmp/rpm-tmp.40833 (%build)
Build time for lkc: 1 seconds

Failed building
Died at ./ltib line 1380.
traceback:
 main::build_host_rpms:1380
  main::host_checks:1435
   main:542

I have a document titled "Ubuntu 11.10 64-Bit host, i.MX53 START_R LTIB 11.09.01 Installation" by Curtis Wald. Will this patch he describes work for Ubuntu 12.04 as well?

Labels (1)
0 Kudos
Reply
2 Replies

719 Views
ShaneKaiser
Contributor II

Thanks for the reply Yuri.

I tried the Ubuntu 11.10 LTIB patch and it works for Ubuntu 12.04.

I have the 64-bit version.

0 Kudos
Reply

719 Views
Yuri
NXP Employee
NXP Employee

Yes, please use "Ubuntu 11.10 64-bit host  i.MX53 START_R LTIB 11.09.01 Installation" - it works for the 12.04 - at least for
32-bit case.

Looks like the problem relates to the lkc package. Please try recommendations in section 9.3.2 (Patch Packages) of the mentioned installation document.

0 Kudos
Reply