Uboot splash screen is not enough, info for kernel bootsplash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Uboot splash screen is not enough, info for kernel bootsplash

ソリューションへジャンプ
1,883件の閲覧回数
mirogliopaolo
Contributor II

I'm using the u-boot bootsplash but is lousy as no kernel loading iteraction is possible:

-no loading scrolling bar

-boot console must be totally hidden or totally shown

On x86 systems i used some years ago a bootsplash composed by scripts and kernel driver, it worked perfectly, because it was possible to press ESC key to show the underlying console and also to send to /dev/splash a message or the progressbar status.

Somebody is using similar system?

If not i will try a porting of that (it was running on LFS).

Best Regards

Miroglio

ラベル(4)
タグ(3)
0 件の賞賛
返信
1 解決策
1,585件の閲覧回数
juangutierrez
NXP Employee
NXP Employee

These features are provided by a separate splashutils package which is a set of userspace scripts and kernel patches, however this package is not maintained by FSL.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,586件の閲覧回数
juangutierrez
NXP Employee
NXP Employee

These features are provided by a separate splashutils package which is a set of userspace scripts and kernel patches, however this package is not maintained by FSL.

0 件の賞賛
返信
1,585件の閲覧回数
mirogliopaolo
Contributor II

Dear Juan,

thank you very much for the answer, that's what i was looking for!

Regards

Miroglio Paolo

0 件の賞賛
返信