Uboot splash screen is not enough, info for kernel bootsplash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Uboot splash screen is not enough, info for kernel bootsplash

Jump to solution
1,421 Views
mirogliopaolo
Contributor II

I'm using the u-boot bootsplash but is lousy as no kernel loading iteraction is possible:

-no loading scrolling bar

-boot console must be totally hidden or totally shown

On x86 systems i used some years ago a bootsplash composed by scripts and kernel driver, it worked perfectly, because it was possible to press ESC key to show the underlying console and also to send to /dev/splash a message or the progressbar status.

Somebody is using similar system?

If not i will try a porting of that (it was running on LFS).

Best Regards

Miroglio

Labels (4)
Tags (3)
0 Kudos
Reply
1 Solution
1,123 Views
juangutierrez
NXP Employee
NXP Employee

These features are provided by a separate splashutils package which is a set of userspace scripts and kernel patches, however this package is not maintained by FSL.

View solution in original post

0 Kudos
Reply
2 Replies
1,124 Views
juangutierrez
NXP Employee
NXP Employee

These features are provided by a separate splashutils package which is a set of userspace scripts and kernel patches, however this package is not maintained by FSL.

0 Kudos
Reply
1,123 Views
mirogliopaolo
Contributor II

Dear Juan,

thank you very much for the answer, that's what i was looking for!

Regards

Miroglio Paolo

0 Kudos
Reply