Uboot SDRAM output drive strength for IMX6D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Uboot SDRAM output drive strength for IMX6D

2,066 Views
tomsaluzzo
Contributor III

Using the IMX6D. Why does Uboot 2009.08 set the output drive strength for DDR3 SDRAM interface signals to 40 ohms? The Micron MT4J128M16HA-15E DDR3 SDRAM datasheet (page 134) states that 34 ohms is the primary output driver impedance setting for DDR3 SDRAM devices.

0 Kudos
Reply
3 Replies

1,809 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tom

34 ohms (more powerful output) provides more noise to board

than 40 ohms, also this [40 ohms] will allow to decrease overall power consumption.

With 40 ohms DDR tests are passed successfully.

Datasheet gives recommended values which may vary in each particular use case.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,808 Views
tomsaluzzo
Contributor III

You stated “With 34 ohms DDR tests are passed successfully”, but Uboot sets to 40 ohms. Did you mean to say - With 40 ohms DDR tests are passed successfully?

Are you saying either 34 ohms or 40 ohms is appropriate?

Tom Saluzzo

Field Application Engineer

Arrow Electronics

1000 Pittsford Victor Rd. 2nd Floor

Pittsford, NY 14534

585.820.2781

tsaluzzo@arrow.com

www.arrow.com <http://www.arrow.com/>

0 Kudos
Reply

1,808 Views
igorpadykov
NXP Employee
NXP Employee

Yes, with 40 ohms DDR tests are passed successfully.

Best regards

chip

0 Kudos
Reply