Uart on MX53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Uart on MX53

559 Views
alis
Contributor I

Hi,

I'm debugging my board based on the MX53 processor. I'm in troublke with the uart, in my design I need to use a full (8 signals) UART, so I must use the UART1.

My device is a DTE device, when I write a one in the  at DCEDTE bit in the UCFR register, I see the RX pin becoming an output and the TXD pin becoming an input.

This is strange because in the reference manual is written the RXD remain input regardless of whether the UART is in DTE or DCE mode, the same is for the TXD.

 

Anyone had experience with the UART on MX53?

 

Regards,

Giacomo.

Labels (1)
0 Kudos
Reply
0 Replies