UVC Gadget Bind Failure on imx-6.6.23-2.0.0.xml

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UVC Gadget Bind Failure on imx-6.6.23-2.0.0.xml

ソリューションへジャンプ
680件の閲覧回数
yslee_
Contributor I
Hi all,
 
I'm currently testing a composite USB gadget setup (UVC) on an i.MX8MP platform using configfs and a shell script (test.sh). The setup works perfectly on the following NXP BSP branches:
 
SUCCESS : imx-5.4.70-2.3.0.xml (Yocto zeus) — /dev/video1 is created
SUCCESS : imx-5.15.71-2.2.0.xml (Yocto kirkstone) — /dev/video1 is created
 
However, on:
FAIL : imx-6.6.23-2.0.0.xml (Yocto scarthgap)
 
the script fails with the following log:
[test-usb-composite] Creating USB gadget: test
[test-usb-composite] Setting device descriptors...
[test-usb-composite] Setting string descriptors...
[test-usb-composite] Creating configuration...
[test-usb-composite] Creating UVC gadget functionality : uvc.usb0
[test-usb-composite] Binding gadget to UDC: 38100000.usb
configfs-gadget.test gadget.0: uvc: uvc_function_bind()
udc 38100000.usb: failed to start test: -19
UDC core: test: couldn't find an available UDC or it's busy
./test.sh: line 203: echo: write error: Device or resource busy
 
Build info:
Image: imx-image-core
 
Platform: 
i.MX8MP EVK
 
Kernel config (relevant options enabled):
CONFIG_USB_FUNCTIONFS=m
CONFIG_GADGET_UAC1=y
CONFIG_GADGET_UAC1_LEGACY=y
CONFIG_USB_G_WEBCAM=m
CONFIG_USB_G_HID=m
CONFIG_USB_VIDEO_CLASS=y
Observations:
No /dev/video1 appears.
 
Script and function registration steps are identical across all tests.
Only this BSP (6.6.23) exhibits the binding failure.
 
Questions:
Has anyone encountered this with the 6.6.23 BSP?
Is there a missing dependency or patch for uvc_function_bind() in this version?
Is this a known regression, or does UVC gadget support require additional configuration in this kernel?
Any suggestions or solutions would be greatly appreciated.
 
Thanks,
 
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
640件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi 

This script can work.

Best Regards,
Zhiming

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
641件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi 

This script can work.

Best Regards,
Zhiming

0 件の賞賛
返信