UUU with Windows 10 Failure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UUU with Windows 10 Failure

1,079 次查看
apie
Contributor I

Hi,

 

i have a short uuu script that works well on Linux with I.MX6 Board.

The contents of the script are as follows:


SDP: boot -f bootloader/u-boot-dtb-stage0.imx
FB: flash 1:0 bootloader/boot.img
FB: done

In production we have to use a windows 10 maschine but i cant get it working.

Steps taken so far:
I Downloaded the uuu tool here:
https://github.com/NXPmicro/mfgtools/releases

Step one (flashing bootloader to ram) always works. FB: commands first threw the error:
Error opening usb device

After installing libusb and creating a driver for the Device i am now stuck with the error:

Error: Failure claim Interface

apie_1-1652343318174.jpeg

 

 

 

0 项奖励
回复
0 回复数