UUU on iMX6DL: UDC device or resource busy?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UUU on iMX6DL: UDC device or resource busy?

2,352 次查看
rakesh3
Contributor V

Dear NXP,

 

I am using the imx6d board and using the UUU tool to flash the image into the board but while flashing and using the FBK command while booting i am getting below error while executing the linuxrc file 

 

Start handle command
udc-core: couldn't find an available UDC or it's busy
./linuxrc: line 143: echo: write error: Device or resource busy
uuc /dev/utp
uuc 0.6 [built Nov  7 2019 19:25:07]
UTP: Waiting for /dev/utp to appear
UTP: file/device node /dev/utp already exists

below is my u-boot configuration.

ONFIG_CMD_FASTBOOT=y
CONFIG_USB_FUNCTION_FASTBOOT=y
CONFIG_USB_GADGET=y
CONFIG_USB_GADGET_DOWNLOAD=y
CONFIG_USB_GADGET_MANUFACTURER="FSL"
CONFIG_USB_GADGET_VENDOR_NUM=0x0525
CONFIG_USB_GADGET_PRODUCT_NUM=0xa4a5
CONFIG_CI_UDC=y 
CONFIG_FSL_FASTBOOT=y
CONFIG_FASTBOOT=y
CONFIG_FASTBOOT_BUF_ADDR=0x83800000 # Address need change according ←-
system, generally it can be the same as ${LOADADDR}
CONFIG_FASTBOOT_BUF_SIZE=0x40000000
CONFIG_FASTBOOT_FLASH=y
CONFIG_FASTBOOT_FLASH_MMC_DEV=1
CONFIG_EFI_PARTITION=y
CONFIG_ANDROID_BOOT_IMAGE=y

I have done below kernel configuration .

CONFIG_USB_CONFIGFS_F_FS=y

CONFIG_USB_CONFIGFS_MASS_STORAGE=y

CONFIG_USB_F_MASS_STORAGE=y

CONFIG_USB_F_FS=y

CONFIG_USB_CONFIGFS_F_FS=y

below is my linuxrc file content

#!/bin/sh
export PATH=/sbin:/bin:/usr/sbin:/usr/bin

mount -t sysfs none /sys
mount -t proc none /proc
mount -t devtmpfs none /dev
mount -t configfs none /sys/kernel/config

modprobe sysflags

# disable turn off display
echo -e "\033[9;0]" > /dev/tty0

#mkdir -p /myconf/config/usb_gadget/g1
#cd /myconf/config/usb_gadget/g1
mkdir -p /sys/kernel/config/usb_gadget/g1
cd /sys/kernel/config/usb_gadget/g1

echo 0x066F > idVendor
echo 0x9BFF > idProduct
mkdir -p strings/0x409
echo 0000000000000000 > strings/0x409/serialnumber
echo "FSL i.MX Board" > strings/0x409/product
mkdir -p configs/c.1
echo 5 > configs/c.1/MaxPower

mkdir os_desc
echo 1 > os_desc/use
echo "MSFT100" > os_desc/qw_sign
echo 0x40 > os_desc/b_vendor_code

mkdir -p functions/ffs.utp
mkdir  /dev/usb-utp
mount -t functionfs utp /dev/usb-utp
ln -s functions/ffs.utp configs/c.1/
ln -s configs/c.1 os_desc

echo /fat > functions/mass_storage.1/lun.0/file

ufb /dev/usb-utp$2/ep0 &

echo run utp at /dev/usb-utp$2/ep0;
while [ ! -e /dev/usb-utp$2/ep1 ]
do
echo "."
sleep 1;
done

echo $1 > UDC  ===> this is the line 143

Please help me on this issue , where i misconfigure the kernel in this .

Attaching the linuxrc file.

Regards,

Rakesh

标签 (3)
标记 (1)
0 项奖励
回复
3 回复数

2,336 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Could you share the script or commands that you are using?
Also, which BSP version are you working with?

Best regards,
Aldo.

0 项奖励
回复

2,331 次查看
rakesh3
Contributor V

Hi Aldo, 

I am using the below script as linuxrc .

#!/bin/sh
export PATH=/sbin:/bin:/usr/sbin:/usr/bin

mount -t sysfs none /sys
mount -t proc none /proc
mount -t devtmpfs none /dev
mount -t configfs none /sys/kernel/config

cmdline=`cat /proc/cmdline`

# disable turn off display
echo -e "\033[9;0]" > /dev/tty0


last=0;

UDC_DIR=/sys/class/udc

function launch_dhcpd() {

touch -f /var/lib/misc/udhcpd.leases
echo start 168.1.1.50 > /conf
echo end 168.1.1.253 >> /conf
echo interface usb$1 >>/conf

ifconfig usb$1 168.1.1.1
udhcpd /conf

}

function contains() {
for i in "${files[@]}"
do
if [ "$i" == "$1" ]; then
return 1;
fi
done
return 0
}

function launch_uuc() {
echo $1 $2
mkdir /sys/kernel/config/usb_gadget/$1
cd /sys/kernel/config/usb_gadget/$1
echo 0x066F > idVendor

if [[ ${cmdline} == *nfsroot* ]]; then
echo 0x9CFF > idProduct
else
echo 0x9BFF > idProduct
fi

mkdir strings/0x409

if [ -e /sys/devices/soc0/soc_uid ]; then
cat /sys/devices/soc0/soc_uid > strings/0x409/serialnumber
else
echo 0000000000000000 > strings/0x409/serialnumber
fi

echo "FSL i.MX Board" > strings/0x409/product
mkdir configs/c.1
echo 5 > configs/c.1/MaxPower

echo ffs.utp$2

echo 1 > os_desc/use
echo "MSFT100" > os_desc/qw_sign
echo 0x40 > os_desc/b_vendor_code

if [[ ${cmdline} == *nfsroot* ]]; then
mkdir functions/ncm.1
ln -s functions/ncm.1 configs/c.1/
# mkdir functions/acm.1
# ln -s functions/acm.1 configs/c.1/
echo $1 > UDC

echo "Start config network"

ifconfig usb$2 up
while [ ! -e /find_one ]
do
if [[ `ifconfig usb$2` == *inet6* ]]; then
break;
fi
sleep 1
done

if [ -e /find_one ]; then
exit 0
fi

touch /find_one

launch_dhcpd $2

remote=""
while [[ "$remote" == "" ]];
do
sleep 2
echo retry get remote ipaddress
ping6 -c2 -I usb$2 ff02::1

remote=`ip -6 neighbor show dev usb$2`
remote=(${remote})
remote=${remote[0]}
done

nfs=${cmdline#*nfsroot=}
nfs=($nfs)
nfs=${nfs[0]}

nfs=${nfs##*:}

echo ${remote} ${nfs}

mount -t nfs [${remote}%usb$2]:${nfsroot}/${nfs} /mnt/

cd /

touch /exit_scan

else
mkdir functions/ffs.utp$2
mkdir /dev/usb-utp$2
mount -t functionfs utp$2 /dev/usb-utp$2
ln -s functions/ffs.utp$2 configs/c.1/
ln -s configs/c.1 os_desc

mkdir functions/mass_storage.1
ln -s functions/mass_storage.1 configs/c.1/
echo /fat > functions/mass_storage.1/lun.0/file

ufb /dev/usb-utp$2/ep0 &

echo run utp at /dev/usb-utp$2/ep0;
while [ ! -e /dev/usb-utp$2/ep1 ]
do
echo "."
sleep 1;
done

echo $1 > UDC

if [ $2 == "0" ]; then
echo uuc /dev/utp
uuc /dev/utp &
else
echo uuc /dev/utp$2
uuc /dev/utp$2 &
fi
fi

return 0;

}

while true; do
if test "$(ls -A "$UDC_DIR")"; then
cd $UDC_DIR
for entry in *
do
if contains $entry; then
files[$last]=$entry;
id=$last;
last=`expr $last + 1`;
echo "Found New UDC: $entry";
launch_uuc $entry $id &
fi

done
sleep 1
else
echo "No udc Available!"
sleep 30
fi

if [ -e /exit_scan ]; then
echo find one active ncm
exec switch_root /mnt /sbin/init
exit 1;
fi

done

echo bye

Here i am using the kernel version 5.10 and u-boot 2021. 

Here error is coming at command "echo $1 > UDC"

Regards,

Rakesh

0 项奖励
回复

2,322 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

thank you for sharing more information, have you tried using the UUU script to flash using Linux kernel?
https://github.com/nxp-imx/mfgtools/wiki/Sample-script#burn-yocto-image-to-emmc-by-linux-kernel

Best regards,
Aldo.

0 项奖励
回复