Hi,
We have a custom i.mx 8m nano board that we are trying to bring up. It very closely follows the DDR4 EVK with a couple of notable differences.
We can successfully run the DDR memory tool - calibration and stress. I've applied the ddr4_timing changes in the u-boot build.
However, when we attempt to burn the emmc from UUU, we see an HID(w):LIBUSB_ERROR_TIMEOUT (after a brief run to 3% - if that really is doing something). The same toolchain is used to burn the LPDDR4 EVK, so I don't think it's a driver issue (but I'm wrong often!).
Any ideas we could try? I'd appreciate any suggestions and can supply more info as needed. Best,
Kipp
Hello everyone,
We are debugging a custom iMX8MP board which is very similar to iMX8MP_DDR4_EVK. The first issue we've come accross is this horrible:
Wait for Known USB Device Appear...
New USB Device Attached at 1:52
1:52>Start Cmd:SDPS: boot -f "flash.bin"
1:52>Fail HID(W):LIBUSB_ERROR_TIMEOUT(1s)
After reading this entry carefully I have understood that just changing the UART setup from UART2 to UART3 this "LIBUSB_ERROR_TIMEOUT" just disappeared. Am i wrong @kippowens ? It seems quite a bit strange as the original error seems to have something to do with USB.
Please @kippowens , could you explain more in detail which changes fixed your problem?
As I am in very similar situation that would very helpful to me.
Thanks in advance!
@AlfTeleco - apologies for not seeing this until now!
The USB timeout issue pops up for a bunch of reasons -- not all are related to the USB directly.
I've seen this...
Hopefully you're long past this and things are working great! Apologies again for the slow response!
Best,
Kipp
I should note as well that I believe I have made all necessary changes to appropriately move the console to UART3 (in u-boot and the yocto kernel), but have yet to see any life on that side of things.
Hello,
If it is not printing maybe changes to UART were not done properly, you may take a look to this guide here for reference:
https://community.nxp.com/t5/i-MX-Community-Articles/How-to-Change-i-MX8MM-evk-Linux-Debug-UART/ba-p...
Also, please check that you have disabled the type-c correctly in uboot defconfig
CONFIG_USB_TCPC=n
And remove the typec_ptn5110 1/2 dependencies in dts
&usbotg1 {
status = "okay";
};
&usbotg2 {
status = "okay";
};
Best regards,
Aldo.
Appreciate the response!
I decided I'd start from the basics and try to move the u-boot console output of the imx8mn nano evk (lpddr4) from UART2 to UART3. My attempts are leading to the same issue I'm seeing on our custom board. Which...I guess...is promising?
Here are the changes I've made to try to move the console to UART3.
Physical Changes:
U-Boot-Imx Device Tree Changes
Imx-Atf Changes:
Optee Changes:
The result when I try to use uuu:
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.127-0-g08c58c9
Success 0 Failure 1
1:222 1/ 2 [HID(W):LIBUSB_ERROR_TIMEOUT ] SDPS: boot -f "imx-boot-imx8mnevk-emmc.bin-flash_evk"
c:\NXP_images_sdk_tools\images\custom>uuu_1.4.127.exe -v imx-boot-imx8mnevk-emmc.bin-flash_evk
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.127-0-g08c58c9
Build in config:
Pctl Chip Vid Pid BcdVersion
==================================================
SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]
SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]
SDPS: MX8DXL 0x1fc9 0x0147
SDPS: MX28 0x15a2 0x004f
SDPS: MX815 0x1fc9 0x013e
SDPS: MX865 0x1fc9 0x0146
SDPS: MX8ULP 0x1fc9 0x014a
SDPS: MX8ULP 0x1fc9 0x014b
SDP: MX7D 0x15a2 0x0076
SDP: MX6Q 0x15a2 0x0054
SDP: MX6D 0x15a2 0x0061
SDP: MX6SL 0x15a2 0x0063
SDP: MX6SX 0x15a2 0x0071
SDP: MX6UL 0x15a2 0x007d
SDP: MX6ULL 0x15a2 0x0080
SDP: MX6SLL 0x1fc9 0x0128
SDP: MX7ULP 0x1fc9 0x0126
SDP: MXRT106X 0x1fc9 0x0135
SDP: MX8MM 0x1fc9 0x0134
SDP: MX8MQ 0x1fc9 0x012b
SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]
SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]
SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]
SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]
SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]
FBK: 0x066f 0x9afe
FBK: 0x066f 0x9bff
FB: 0x0525 0xa4a5
FB: 0x18d1 0x0d02
FB: 0x3016 0x0001
Wait for Known USB Device Appear...
New USB Device Attached at 1:222
1:222>Start Cmd:SDPS: boot -f "imx-boot-imx8mnevk-emmc.bin-flash_evk"
10%1:222>Fail HID(W):LIBUSB_ERROR_TIMEOUT(1.045s)
This change:
Stops UUU from loading the bootloader...
Is it possible this points to the need for a change in optee?
Hello,
Good to know that you have made some progress in your issue, I notice that you haven't changed IMX_BOOT_UART_BASE definition in ATF:
https://source.codeaurora.org/external/imx/imx-atf/tree/plat/imx/imx8m/imx8mn/include/platform_def.h...
Please check this as well
Best regards,
Aldo.
Thank you for the response, Aldo.
I did have that change in there and I was able to get things working on my custom board (never did get things completely working on UART3 on the EVK, but that's ok!).
I'm still struggling to boot directly from emmc, but I'll post that as a separate topic. Thank you again!
Kipp
I'm now able to run UUU and burn to emmc correctly, it appears. I was not properly initializing the clock for UART3.
HOWEVER...I still am not getting any debug output on UART3 (during u-boot).