UUU does not return after writing images

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UUU does not return after writing images

ソリューションへジャンプ
2,750件の閲覧回数
tanoue
Contributor III

I wrote images to i.MX 8M Plus EVK with UUU.

However, UUU does not return after writing images.

 

My procedures is here.

1. Build image with "Linux 5.15.32_2.0.0" according to i.MX Yocto Project User's Guide(Rev. LF5.15.32_2.0.0 — 12 July 2022)

repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.32-2.0.0.xml

2. After build, write images(.bin-flash_evk and .wic.bz2) to EVK using the following command.

sudo ./uuu -b emmc_all imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk imx-image-full-imx8mp-lpddr4-evk.wic.bz2

3. The following message shown and stop writting images. UUU did not return after writing .bin-flash_evk and .wic.bz2 was not written to EVK.

uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.165-0-ge10b026

Success 0 Failure 0


1:8 1/ 1 [=================100%=================] SDPS: boot -scanterm -f /<path>/imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk

 

What should I do.

 

Best regards.

tanoue.

0 件の賞賛
返信
1 解決策
2,667件の閲覧回数
tanoue
Contributor III

My problem was solved with using next stable uuu(1.4.193).

However, I didn't understand which changes solved my problem.

 

Please, let me know.

 

Best regards.

tanoue.

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
2,736件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Please run the tool in verbose mode by using the following command:
sudo ./uuu -V -b emmc_all imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk imx-image-full-imx8mp-lpddr4-evk.wic.bz2

After this, please share the tool output so I can see more information on what is going on.
Also, please share the serial terminal (Uboot) log.

Best regards,
Aldo.

0 件の賞賛
返信
2,729件の閲覧回数
tanoue
Contributor III

Hi, @AldoG 

Thank you for your reply.

I did it and attached log that has UUU and Uboot output.

Please, see it.

 

Best regards.

tanoue.

0 件の賞賛
返信
2,709件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

This seems to be a problem when using Ubuntu 20.04/libusb, unfortunately haven't found what is actually going wrong, more details here:
https://github.com/NXPmicro/mfgtools/issues/183

Some workarounds that have worked for other customers that you could try on your side are:
> Using Ubuntu 18.04 host PC
> Do not use USB Hub, connect directly to host PC
> Even connecting to a different USB port has helped in some cases

Please try any of the above if it can help you, if not please do let me know.

Best regards,
Aldo.

0 件の賞賛
返信
2,680件の閲覧回数
tanoue
Contributor III

Hi, @AldoG 

 

I tried it again on Ubuntu 18.04 host PC without USB Hub.

However, its result was same.

I attached log.

 

Best regards.

tanoue.

0 件の賞賛
返信
2,668件の閲覧回数
tanoue
Contributor III

My problem was solved with using next stable uuu(1.4.193).

However, I didn't understand which changes solved my problem.

 

Please, let me know.

 

Best regards.

tanoue.

0 件の賞賛
返信
2,648件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hi,

Glad to hear that it is now working, unfortunately is hard for me to say what actually fixed your issue since device got stuck at Run fastboot…. So, it could be some random USB issue.

Finally, from the release notes the bug fixes between those 2 versions are the following:
https://github.com/NXPmicro/mfgtools/wiki/Release-Notes#bug-fixes-1

Bug fixes
Fixed 314 Corrupt image with larger transfer sizes at sdp(s)
Fixed missed true at else branch at built-in fat_write script and nand_burn_loader
Fixed invalid progress percentage in verbose mode
Fixed QSPI flashing script
Fix #297 print error when run quit cmd in shell mode
Fix #180 support check getval return value

Best regards,
Aldo.

0 件の賞賛
返信
2,628件の閲覧回数
tanoue
Contributor III

Hi, @AldoG 

Thank your for your replying.

I understood your opinion.

Anyway, I hope this topic helps someone with the same problem.

0 件の賞賛
返信