I wrote images to i.MX 8M Plus EVK with UUU.
However, UUU does not return after writing images.
My procedures is here.
1. Build image with "Linux 5.15.32_2.0.0" according to i.MX Yocto Project User's Guide(Rev. LF5.15.32_2.0.0 — 12 July 2022)
repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.32-2.0.0.xml
2. After build, write images(.bin-flash_evk and .wic.bz2) to EVK using the following command.
sudo ./uuu -b emmc_all imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk imx-image-full-imx8mp-lpddr4-evk.wic.bz2
3. The following message shown and stop writting images. UUU did not return after writing .bin-flash_evk and .wic.bz2 was not written to EVK.
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.165-0-ge10b026
Success 0 Failure 0
1:8 1/ 1 [=================100%=================] SDPS: boot -scanterm -f /<path>/imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk
What should I do.
Best regards.
tanoue.
Solved! Go to Solution.
My problem was solved with using next stable uuu(1.4.193).
However, I didn't understand which changes solved my problem.
Please, let me know.
Best regards.
tanoue.
Hello,
Please run the tool in verbose mode by using the following command:
sudo ./uuu -V -b emmc_all imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk imx-image-full-imx8mp-lpddr4-evk.wic.bz2
After this, please share the tool output so I can see more information on what is going on.
Also, please share the serial terminal (Uboot) log.
Best regards,
Aldo.
Hi, @AldoG
Thank you for your reply.
I did it and attached log that has UUU and Uboot output.
Please, see it.
Best regards.
tanoue.
Hello,
This seems to be a problem when using Ubuntu 20.04/libusb, unfortunately haven't found what is actually going wrong, more details here:
https://github.com/NXPmicro/mfgtools/issues/183
Some workarounds that have worked for other customers that you could try on your side are:
> Using Ubuntu 18.04 host PC
> Do not use USB Hub, connect directly to host PC
> Even connecting to a different USB port has helped in some cases
Please try any of the above if it can help you, if not please do let me know.
Best regards,
Aldo.
Hi, @AldoG
I tried it again on Ubuntu 18.04 host PC without USB Hub.
However, its result was same.
I attached log.
Best regards.
tanoue.
My problem was solved with using next stable uuu(1.4.193).
However, I didn't understand which changes solved my problem.
Please, let me know.
Best regards.
tanoue.
Hi, 
Glad to hear that it is now working, unfortunately is hard for me to say what actually fixed your issue since device got stuck at Run fastboot…. So, it could be some random USB issue.
Finally, from the release notes the bug fixes between those 2 versions are the following:
https://github.com/NXPmicro/mfgtools/wiki/Release-Notes#bug-fixes-1
Bug fixes
Fixed 314 Corrupt image with larger transfer sizes at sdp(s)
Fixed missed true at else branch at built-in fat_write script and nand_burn_loader
Fixed invalid progress percentage in verbose mode
Fixed QSPI flashing script
Fix #297 print error when run quit cmd in shell mode
Fix #180 support check getval return value
Best regards,
Aldo.
Hi, @AldoG
Thank your for your replying.
I understood your opinion.
Anyway, I hope this topic helps someone with the same problem.