Hi all:
I encountered a flash failure when flash Android 10 image to imx8q demo board through UUU tool under Windows7。
However, I flash Android 9 image in the same environment and it was successful. And I was also successful in flashing Android 10 image under window10.
Doesn't it support flash Android10 image under window7?
Are there any brothers who have encountered the same problem? How is it solved?
I tried several UUU versions recently. The phenomenon is the same. It doesn't necessarily need to be downloaded under win7. I just used to use win7 and don't want to change the system, so I came to the community to ask if there are other ways. If it is determined that win7 does not support, then I can only change the system, Thank you for your answer