UUU FBK command is not working in imx6s

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UUU FBK command is not working in imx6s

4,564件の閲覧回数
hangunwoo
Contributor II

Hello.

I have a problem with my customized imx6solo board.

I built the yocto(zeus) and fusing the u-boot, kernel image with initramfs.

And also built the initramfs in my zeus yocto.

Everything is okay, but FBK command is not working in UUU.

I changed the kernel image and initramfs in L4.19.35_1.1.0_images_MX6QPDLSOLOX.zip

But  FBK command is still not working.

Is the FBK command not supported on the mx6solo or mx6 series?

here is my uuu script.

-----------------

uuu_version 1.2.39

# boot from u-boot-dtb.imx
# load the u-boot image into the sdram
SDP: boot -f firmware/u-boot-dtb.imx

# burn u-boot to emmc
# macro value is follow the u-boot source
FB: ucmd setenv fastboot_dev mmc
FB: ucmd setenv mmcdev ${emmc_dev}
FB: ucmd mmc dev ${emmc_dev}
FB: flash bootloader firmware/u-boot-dtb.imx
FB: ucmd mmc partconf ${emmc_dev} 1 1 0

# load kernel & initram filesystem
FB: ucmd setenv fastboot_buffer ${loadaddr}
FB: download -f firmware/zImage
FB: ucmd setenv fastboot_buffer ${fdt_addr}
FB: download -f firmware/u-boot.dtb
FB: ucmd setenv fastboot_buffer ${initrd_addr}
FB: download -f firmware/fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot
FB: ucmd setenv mfgtool_args ${mfgtool_args} mfg_mmcdev=${emmc_dev}
FB: ucmd run mfgtool_args
FB: acmd ${kboot} ${loadaddr} ${initrd_addr} ${fdt_addr}

# get mmc dev number from kernel command line
FBK: ucmd cmdline=`cat /proc/cmdline`;cmdline=${cmdline#*mfg_mmcdev=};cmds=($cmdline);echo ${cmds[0]}>/tmp/mmcdev
# Wait for mmc
FBK: ucmd mmc=`cat /tmp/mmcdev`; while [ ! -e /dev/mmcblk${mmc} ]; do sleep 1; echo "wait for /dev/mmcblk${mmc} appear"; done;

FBK: Done

-------------------

This is uuu verbose log.

--------------------

frank@frank-desktop:~/DEV/uuu-1.3.191/output$ sudo ./uuu -v fusing.auto
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.3.191-0-g4fe24b9

Build in config:
    Pctl     Chip         Vid     Pid     BcdVersion
    ==================================================
    SDPS:     MX8QXP         0x1fc9     0x012f     [0x0002..0xffff]
    SDPS:     MX8QM         0x1fc9     0x0129     [0x0002..0xffff]
    SDPS:     MX8DXL         0x1fc9     0x0147
    SDPS:     MX28         0x15a2     0x004f
    SDPS:     MX815         0x1fc9     0x013e
    SDPS:     MX865         0x1fc9     0x0146
    SDP:     MX7D         0x15a2     0x0076
    SDP:     MX6Q         0x15a2     0x0054
    SDP:     MX6D         0x15a2     0x0061
    SDP:     MX6SL         0x15a2     0x0063
    SDP:     MX6SX         0x15a2     0x0071
    SDP:     MX6UL         0x15a2     0x007d
    SDP:     MX6ULL         0x15a2     0x0080
    SDP:     MX6SLL         0x1fc9     0x0128
    SDP:     MX7ULP         0x1fc9     0x0126
    SDP:     MXRT106X     0x1fc9     0x0135
    SDP:     MX8MM         0x1fc9     0x0134
    SDP:     MX8MQ         0x1fc9     0x012b
    SDPU:     SPL         0x0525     0xb4a4     [0x0000..0x04ff]
    SDPV:     SPL1         0x0525     0xb4a4     [0x0500..0x9998]
    SDPU:     SPL         0x0525     0xb4a4     [0x9999..0x9999]
    SDPU:     SPL         0x3016     0x1001     [0x0000..0x04ff]
    SDPV:     SPL1         0x3016     0x1001     [0x0500..0x9998]
    FBK:              0x066f     0x9afe
    FBK:              0x066f     0x9bff
    FB:              0x0525     0xa4a5
    FB:              0x18d1     0x0d02
    FB:              0x3016     0x0001
Wait for Known USB Device Appear...
New USB Device Attached at 1:1
1:1>Start Cmd:SDP: boot -f firmware/u-boot-dtb.imx
6400%1:1>Okay (0.635s)
New USB Device Attached at 1:1
1:1>Start Cmd:FB: ucmd setenv fastboot_dev mmc
1:1>Okay (0.001s)
1:1>Start Cmd:FB: ucmd setenv mmcdev ${emmc_dev}
1:1>Okay (0.172s)
1:1>Start Cmd:FB: ucmd mmc dev ${emmc_dev}
1:1>Okay (0.092s)
1:1>Start Cmd:FB: flash bootloader firmware/u-boot-dtb.imx
0x100000001:1>Okay (0.165s)
1:1>Start Cmd:FB: ucmd mmc partconf ${emmc_dev} 0 1 0
1:1>Okay (0.003s)
1:1>Start Cmd:FB: ucmd setenv fastboot_buffer ${loadaddr}
1:1>Okay (0s)
1:1>Start Cmd:FB: download -f firmware/zImage
1:1>Okay (0.235s)
1:1>Start Cmd:FB: ucmd setenv fastboot_buffer ${fdt_addr}
1:1>Okay (0.001s)
1:1>Start Cmd:FB: download -f firmware/u-boot.dtb
1:1>Okay (0.008s)
1:1>Start Cmd:FB: ucmd setenv fastboot_buffer ${initrd_addr}
1:1>Okay (0s)
1:1>Start Cmd:FB: download -f firmware/fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot
1:1>Okay (0.397s)
1:1>Start Cmd:FB: acmd ${kboot} ${loadaddr} ${initrd_addr} ${fdt_addr}
1:1>Okay (0s)

And attached the booting log.

------------------------

U-Boot 2019.04-lf-5.4.y_v2019.04+g228843cdf5 (Jun 22 2020 - 17:24:36 +0900)s

CPU:   Freescale i.MX6SOLO rev1.3 996 MHz (running at 792 MHz)
CPU:   Extended Commercial temperature grade (-20C to 105C) at 41C
Reset cause: POR
Model: Freescale i.MX6 DualLite SABRE Smart Device Board
Board: MX6-SabreSD
I2C:   ready
DRAM:  512 MiB
MMC:   FSL_SDHC: 1, FSL_SDHC: 2, FSL_SDHC: 3
Loading Environment from MMC... MMC: no card present
*** Warning - No block device, using default environment

No panel detected: default to HDMI
Display: HDMI (1024x768)
In:    serial
Out:   serial
Err:   serial
MMC: no card present
flash target is MMC:2
MMC: no card present
MMC card init failed!
MMC: no card present
** Block device MMC 2 not supported
Net:   Board Net Initialization Failed
No ethernet found.
Fastboot: Normal
Boot from USB for mfgtools
*** Warning - Use default environment for                                mfgtools
, using default environment

Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; el
se bootz ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;

## Checking Image at 12c00000 ...
Unknown image format!
Run fastboot ...
flash target is MMC:3
switch to partitions #0, OK
mmc3(part 0) is current device
Starting download of 719872 bytes
.....
downloading of 719872 bytes finished
writing to partition 'bootloader'
Initializing 'bootloader'
switch to partitions #1, OK
mmc3(part 1) is current device
Writing 'bootloader'

MMC write: dev # 3, block # 2, count 1406 ... 1406 blocks written: OK
Writing 'bootloader' DONE!
Starting download of 7300424 bytes
.......................................................
downloading of 7300424 bytes finished
Starting download of 53591 bytes

downloading of 53591 bytes finished
Starting download of 12883324 bytes
..........................................................................
........................
downloading of 12883324 bytes finished
Kernel image @ 0x12000000 [ 0x000000 - 0x6f6548 ]
## Loading init Ramdisk from Legacy Image at 12c00000 ...
   Image Name:   fsl-image-mfgtool-initramfs-imx6
   Image Type:   ARM Linux RAMDisk Image (uncompressed)
   Data Size:    12883260 Bytes = 12.3 MiB
   Load Address: 00000000
   Entry Point:  00000000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 18000000
   Booting using the fdt blob at 0x18000000
   Using Device Tree in place at 18000000, end 18010156
No PMIC found!

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 5.4.3+gf8118585ee3c (frank@frank-desktop) (gcc version 9.2.0 (GCC)) #1 SMP PREEMPT Tue Jun 23 12:47:04 KST 2020
[    0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] OF: fdt: Machine model: Freescale i.MX6 DualLite SABRE Smart Device Board
[    0.000000] Memory policy: Data cache writeback
[    0.000000] Reserved memory: created CMA memory pool at 0x1c000000, size 320 MiB
[    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[    0.000000] CPU: All CPU(s) started in SVC mode.
[    0.000000] percpu: Embedded 20 pages/cpu s50600 r8192 d23128 u81920
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 130048
[    0.000000] Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc clk_ignore_unused
[    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes, linear)
[    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes, linear)
[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[    0.000000] Memory: 155588K/524288K available (10240K kernel code, 972K rwdata, 3004K rodata, 1024K init, 6564K bss, 41020K reserved, 327
680K cma-reserved, 0K highmem)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[    0.000000] Running RCU self tests
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu:     RCU lockdep checking is enabled.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
[    0.000000]  Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[    0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[    0.000000] L2C-310 erratum 769419 enabled
[    0.000000] L2C-310 enabling early BRESP for Cortex-A9
[    0.000000] L2C-310 full line of zeros enabled for Cortex-A9
[    0.000000] L2C-310 ID prefetch enabled, offset 16 lines
[    0.000000] L2C-310 dynamic clock gating enabled, standby mode enabled
[    0.000000] L2C-310 cache controller enabled, 16 ways, 512 kB
[    0.000000] L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76450001
[    0.000000] random: get_random_bytes called from start_kernel+0x328/0x4dc with crng_init=0
[    0.000000] Switching to timer-based delay loop, resolution 333ns
[    0.000007] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
[    0.000044] clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
[    0.002048] Console: colour dummy device 80x30
[    0.002090] Lock dependency validator: Copyright (c) 2006 Red Hat, Inc., Ingo Molnar
[    0.002109] ... MAX_LOCKDEP_SUBCLASSES:  8
[    0.002127] ... MAX_LOCK_DEPTH:          48
[    0.002146] ... MAX_LOCKDEP_KEYS:        8192
[    0.002162] ... CLASSHASH_SIZE:          4096
[    0.002180] ... MAX_LOCKDEP_ENTRIES:     32768
[    0.002195] ... MAX_LOCKDEP_CHAINS:      65536
[    0.002212] ... CHAINHASH_SIZE:          32768
[    0.002230]  memory used by lock dependency info: 3997 kB
[    0.002245]  memory used for stack traces: 2112 kB
[    0.002262]  per task-struct memory footprint: 1536 bytes
[    0.002360] Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
[    0.002388] pid_max: default: 32768 minimum: 301
[    0.002753] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes, linear)
[    0.002783] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes, linear)
[    0.006003] CPU: Testing write buffer coherency: ok
[    0.006116] CPU0: Spectre v2: using BPIALL workaround
[    0.007643] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.059652] Setting up static identity map for 0x10100000 - 0x10100060
[    0.079541] rcu: Hierarchical SRCU implementation.
[    0.119547] smp: Bringing up secondary CPUs ...
[    0.200086] smp: Brought up 1 node, 1 CPU
[    0.200115] SMP: Total of 1 processors activated (6.00 BogoMIPS).
[    0.200136] CPU: All CPU(s) started in SVC mode.
[    0.202369] devtmpfs: initialized
[    0.239398] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[    0.250015] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[    0.250086] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[    0.262040] pinctrl core: initialized pinctrl subsystem
[    0.264795] NET: Registered protocol family 16
[    0.287511] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.291016] cpuidle: using governor menu
[    0.291384] CPU identified as i.MX6DL, silicon rev 1.3
[    0.352979] No ATAGs?
[    0.353274] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[    0.353367] hw-breakpoint: maximum watchpoint size is 4 bytes.
[    0.356830] imx6dl-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
[    0.359644] imx mu driver is registered.
[    0.360487] imx rpmsg driver is registered.
[    0.487699] vgaarb: loaded
[    0.489093] SCSI subsystem initialized
[    0.500663] usbcore: registered new interface driver usbfs
[    0.500888] usbcore: registered new interface driver hub
[    0.501239] usbcore: registered new device driver usb
[    0.502854] mc: Linux media interface: v0.10
[    0.502967] videodev: Linux video capture interface: v2.00
[    0.503194] pps_core: LinuxPPS API ver. 1 registered
[    0.503219] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.503283] PTP clock support registered
[    0.529666] imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[    0.533080] mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
[    0.534877] mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
[    0.534906] mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
[    0.535168] MIPI CSI2 driver module loaded
[    0.539066] clocksource: Switched to clocksource mxc_timer1
[    1.207928] VFS: Disk quotas dquot_6.6.0
[    1.208107] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    1.236443] thermal_sys: Registered thermal governor 'step_wise'
[    1.237152] NET: Registered protocol family 2
[    1.239238] tcp_listen_portaddr_hash hash table entries: 256 (order: 1, 10240 bytes, linear)
[    1.239353] TCP established hash table entries: 4096 (order: 2, 16384 bytes, linear)
[    1.239453] TCP bind hash table entries: 4096 (order: 5, 147456 bytes, linear)
[    1.239941] TCP: Hash tables configured (established 4096 bind 4096)
[    1.240326] UDP hash table entries: 256 (order: 2, 20480 bytes, linear)
[    1.240440] UDP-Lite hash table entries: 256 (order: 2, 20480 bytes, linear)
[    1.240889] NET: Registered protocol family 1
[    1.273408] RPC: Registered named UNIX socket transport module.
[    1.273500] RPC: Registered udp transport module.
[    1.273524] RPC: Registered tcp transport module.
[    1.273544] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    1.285057] PCI: CLS 0 bytes, default 64
[    1.286406] Trying to unpack rootfs image as initramfs...
[    2.491431] Freeing initrd memory: 12584K
[    2.492017] hw perfevents: no interrupt-affinity property for /soc/pmu, guessing.
[    2.492503] hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
[    2.495332] Bus freq driver module loaded
[    2.499500] Initialise system trusted keyrings
[    2.500238] workingset: timestamp_bits=30 max_order=17 bucket_order=0
[    2.529770] NFS: Registering the id_resolver key type
[    2.529938] Key type id_resolver registered
[    2.530027] Key type id_legacy registered
[    2.530698] fuse: init (API version 7.31)
[    2.578820] Key type asymmetric registered
[    2.579115] Asymmetric key parser 'x509' registered
[    2.579329] io scheduler mq-deadline registered
[    2.579358] io scheduler kyber registered
[    2.587392] imx6q-pcie 1ffc000.pcie: host bridge /soc/pcie@1ffc000 ranges:
[    2.587601] imx6q-pcie 1ffc000.pcie:    IO 0x01f80000..0x01f8ffff -> 0x00000000
[    2.587819] imx6q-pcie 1ffc000.pcie:   MEM 0x01000000..0x01efffff -> 0x01000000
[    2.601732] imx-sdma 20ec000.sdma: Direct firmware load for imx/sdma/sdma-imx6q.bin failed with error -2
[    2.601838] imx-sdma 20ec000.sdma: Falling back to sysfs fallback for: imx/sdma/sdma-imx6q.bin
[    2.607679] mxs-dma 110000.dma-apbh: initialized
[    2.617166] 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 27, base_baud = 5000000) is a IMX
[    3.397515] printk: console [ttymxc0] enabled
[    3.432770] brd: module loaded
[    3.467434] loop: module loaded
[    3.471849] imx ahci driver is registered.
[    3.482038] spi_imx 2008000.ecspi: probed
[    3.488203] libphy: Fixed MDIO Bus: probed
[    3.492496] CAN device driver interface
[    3.504351] pps pps0: new PPS source ptp0
[    3.509069] fec 2188000.ethernet: Invalid MAC address: 00:00:00:00:00:00
[    3.515815] fec 2188000.ethernet: Using random MAC address: a2:55:37:77:82:2e
[    3.530863] libphy: fec_enet_mii_bus: probed
[    3.537215] fec 2188000.ethernet eth0: registered PHC device 0
[    3.543860] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    3.550490] ehci-pci: EHCI PCI platform driver
[    3.555083] ehci-mxc: Freescale On-Chip EHCI Host driver
[    3.560922] usbcore: registered new interface driver usb-storage
[    3.698220] imx6q-pcie 1ffc000.pcie: Phy link never came up
[    3.707095] imx6q-pcie 1ffc000.pcie: failed to initialize host
[    3.713025] imx6q-pcie 1ffc000.pcie: unable to add pcie port.
[    3.762175] imx_usb 2184200.usb: No over current polarity defined
[    3.772600] ci_hdrc ci_hdrc.1: EHCI Host Controller
[    3.777861] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
[    3.809094] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
[    3.819884] hub 1-0:1.0: USB hub found
[    3.824057] hub 1-0:1.0: 1 port detected
[    3.845172] Mass Storage Function, version: 2009/09/11
[    3.850647] LUN: removable file: (no medium)
[    3.855045] no file given for LUN0
[    3.858759] g_mass_storage ci_hdrc.0: failed to start g_mass_storage: -22
[    3.874801] imx2-wdt 20c0000.wdog: timeout 60 sec (nowayout=0)
[    3.883798] sdhci: Secure Digital Host Controller Interface driver
[    3.890085] sdhci: Copyright(c) Pierre Ossman
[    3.894468] sdhci-pltfm: SDHCI platform and OF driver helper
[    3.902060] sdhci-esdhc-imx 2194000.usdhc: Got CD GPIO
[    3.907299] sdhci-esdhc-imx 2194000.usdhc: Got WP GPIO
[    3.957122] mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
[    3.966428] sdhci-esdhc-imx 2198000.usdhc: Got CD GPIO
[    3.971745] sdhci-esdhc-imx 2198000.usdhc: Got WP GPIO
[    4.020704] mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
[    4.072221] mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
[    4.081356] usbcore: registered new interface driver usbhid
[    4.087071] usbhid: USB HID core driver
[    4.100754] galcore: clk_get vg clock failed, disable vg!
[    4.107611] Galcore version 6.4.0.234062

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

4,393件の閲覧回数
hangunwoo
Contributor II

Okay. I solved this issue in myself. :smileyhappy:

It caued by UDC.

I guess udc is not properly configured in my kernel defconfig and dts file.

The below steps are required for UDC to work properly.

u-boot defconfig

--------------

CONFIG_CI_UDC=y

CONFIG_CMD_FASTBOOT=y
CONFIG_USB_FUNCTION_FASTBOOT=y
CONFIG_FASTBOOT_UUU_SUPPORT=y
CONFIG_FASTBOOT=y
CONFIG_FASTBOOT_BUF_ADDR=0x12000000
CONFIG_FASTBOOT_BUF_SIZE=0x10000000
CONFIG_FASTBOOT_FLASH=y
CONFIG_EFI_PARTITION=y

Kernel defconfig

--------------

CONFIG_USB_CHIPIDEA=y
CONFIG_USB_CHIPIDEA_UDC=y
CONFIG_USB_CHIPIDEA_HOST=y
CONFIG_USB_GADGET=y
CONFIG_USB_MASS_STORAGE=y
CONFIG_USB_FSL_USB2=y
CONFIG_USB_CONFIGFS=y
CONFIG_USB_CONFIGFS_MASS_STORAGE=y
CONFIG_USB_CONFIGFS_F_FS=y

imx6dl-sabresd.dts

--------------

&usbotg {
    dr_mode = "peripheral";
    status = "okay";
};

And i will upload my kernel defconfig for your reference.

Regards.

0 件の賞賛
返信

4,393件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Han

seems fbk is working only with android as described in

sect.5.6 FBK: Android fastboot protocol uuu manual

https://github.com/NXPmicro/mfgtools/releases/download/uuu_1.2.135/UUU.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,393件の閲覧回数
hangunwoo
Contributor II

Thanks for your reply.

I think your comment is wrong.

FB command is the Android fastboot protocol too. But it works fine.

FBK command is the same. It's not support only with android.

I think it depends on initramfs or kernel.

Regards.