USDHC - SDIO on iMX53 vs iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USDHC - SDIO on iMX53 vs iMX6

Jump to solution
4,821 Views
jtobias
Contributor III

Hi All,

I have an iMX53 and iMX6Q Sabre SD dev boards, both boards were running the same kernel based on 3.11-rc7, with same sdhci core, sdhci-esdhc-imx controller for handling USDHC devices. My WIFI module (SD8797)  work on iMX53 (4bit mode) and didn't get any error upon loading the driver but, running it with iMX6 the TIMEOUT bit on INT STATUS register was set when I checked it. The other strange was that if I use different wifi module (atheros), the said module work on iMX6 on 4bit mode.

Any idea, pointers or clue that you can share with me?.

Regards,

john

Labels (2)
1 Solution
2 Replies
1,910 Views
jtobias
Contributor III

Hi Fabio,

It works!!! Thanks again!

Regards,

john

0 Kudos
Reply
1,911 Views
fabio_estevam
NXP Employee
NXP Employee