Hi junya
for PC to be able to recognize i.MX6
i.MX6 should run Linux or put in Serial Downloader
mode. That is it should run some program.
If this is new board one can try to run SDK usb test with jtag:
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for help.
I confirmed that is recognized the i.MX6 in Serial Downloader mode.
Do I need especial software to operate the usb device mode on Linux?