USB2.0 Compliance test (Android)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB2.0 Compliance test (Android)

1,361 次查看
yuhigashino
Contributor I

Hi

I'm developing Embedded Board with i.MX6 Quad in Android (KitKat).

For the USB 2.0 HS compliance test of HOST, tested Board have to generate test packet.

But, I don't know the way.

 

Is there any recommend way for that?

 

if there is, please let me know.

 

thanks

0 项奖励
回复
1 回复

1,019 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yu

usb test mode for compliance test can be implemented using memtool kitkat patch

android-imx6-kitkat/0347-ENGR00222875-1-Lindent-memtools.patch at master · rabeeh/android-imx6-kitka... 

Patch to make i.MX6DQ USB to support test modes for certification test 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复