USB to LAN test for IMX6UL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB to LAN test for IMX6UL

1,250件の閲覧回数
anshulkhare
Contributor III

Hi All,

I have an iMX6UL board,
i am doing U-Boot USB to LAN Test .
is there any command to perform the test in U-Boot

any suggestion to perform the test would be appreciated .

Best Regards,

Anshul

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,072件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Anshul,

I do not think so we have the support for USB Gadget in UBOOT,  only basic MSD, and CDC,  if you want to test the USB to LAN you need to be with the full Linux Support. and you need to have the driver for the USB stick that you are planning to use.

Hope this helps.,  Have a happy new year 2018.

0 件の賞賛
返信

1,072件の閲覧回数
anshulkhare
Contributor III

Hello Jamesbone,

   Thank you for reply. In U-Boot, i am able to find Support for USB Storage device('usb start' command is available),

but i am not able to find the support for Ethernet device via USB(eg: USB to LAN converter).

if any body can help on this that would be helpful for me.

--Anshul

0 件の賞賛
返信