USB storage in u-boot with i.mx287?

cancel
Showing results for 
Search instead for 
Did you mean: 

USB storage in u-boot with i.mx287?

690 Views
latorta
Contributor II

Hi everyone!

I'm trying to use a USB mass storage dongle in u-boot. I would like to load the kernel, the fdt blob and other files from it, but u-boot doesn't detect it. The OS does.

The output I get from u-boot is

CCARDIMX28 # usb start
(Re)start USB...
USB0:   USB EHCI 1.00
scanning bus 0 for devices... 1 USB Device(s) found
       scanning usb for storage devices... 0 Storage Device(s) found
       scanning usb for ethernet devices... 0 Ethernet Device(s) found

I tried different dongles, I set the USB enable pin, I patched u-boot like this -> http://git.denx.de/?p=u-boot.git;a=blobdiff;f=common/usb_hub.c;h=652a104361f63ee715a99e924ccd1145a2c...
but anything changed.
I read that someone can get the usb device detected from u-boot -> https://community.nxp.com/thread/474963 so I don't get why I can't.

Thank you for your help.

Labels (1)
Tags (2)
0 Kudos
2 Replies

438 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Francesco

this may be posted on digi forum Digi Forum 

as seems wrong images was used in the case and card supports usb in uboot as mentioned on

Enable USB Host on ccardimx28 and DEY? - Digi Forum 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

438 Views
latorta
Contributor II

Hi Igor.

Do you think my problem could be just in the u-boot image or should I check other images?

Anyway I'll post on DIGI Forum.

Thank you.

0 Kudos