Please refer to the Chapter 39 of the attached document. Hope it helps.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Did you enable one of these options in the dts?
hnp-enable
srp-enable
Just changing hnp-disable to hnp-enable should do the trick.
However, the a_bus_req/a_bus_drop options do not appear there:
/sys/bus/platform/devices/ci_hdrc.0/inputs/a_bus_req
but rather here for me:
/sys/devices/soc0/soc/2100000.aips-bus/2184000.usb/ci_hdrc.0/inputs/a_bus_req
Gilles.
Hi Gilles Talis,
Yes , the below configurations are updated in the dts file,
hnp-enable
srp-enable
and the a_bus_req node is not present in the path you mentioned in the above reply.
Is there any other requirement needed in 4.1.15 kernel ?
Thanks and Regards
Shravan S
Hi Gilles Talis,
I am able to see the nodes
/sys/devices/soc0/soc/2100000.aips-bus/2184000.usb/ci_hdrc.0/inputs/a_bus_req
as you mentioned in the previous mail.
But the role switching is not happening with my iPhone after the below command
echo 1 > /sys/devices/soc0/soc/2100000.aips-bus/2184000.usb/ci_hdrc.0/inputs/a_bus_req
I am following the procedure as per below
Linux/Documentation/usb/chipidea.txt - Linux Cross Reference - Free Electrons
The Board details : iMx6q sabre Auto infotainment board
Thanks and Regards
Shravan S
Hi Gilles Talis,
Below are the behaviour I am facing during role switching,
1) NXP board is in host mode -By default ( echo host > /sys/kernel/debug/ci.hdrc0/role )
on "lsusb" command I am able to see the devices connected = > Its a expected behaviour.
The connected B-device ( Apple iPhone ) is getting charged.
2) NXP Board is in gadget mode ( echo gadget > /sys/kernel/debug/ci.hdrc0/role )
on "lsusb" command I am not able to see the devices connected = > Its a expected behaviour.
The connected B-device ( Apple iPhone ) is not getting charged. As iPhone expects the power to be supplied from the connected device , when the iPhone is in host mode .
I am suspecting that vbus should be enabled even when the NXP device is in gadget mode .
Did some code modification (short cut way => not the proper fix) to enable to regulator to have the voltage supply in vbus in both the modes . The proper fix should be handling of gpio to enable vbus in both host and device(gadget) modes .
Even after we enable the vbus , we are not able to perform role switch , the nodes responsible for role switch (echo host > /sys/kernel/debug/ci.hdrc0/role) are updating with proper values , but we are not able to see the exact functionality of role switching.
And the documentation part of the kernel say the different nodes for the role switching as below
I am able to see the nodes
/sys/devices/soc0/soc/2100000.aips-bus/2184000.usb/ci_hdrc.0/inputs/a_bus_req
as you mentioned in the document
But the role switching is not happening with my iPhone after the below command
echo 1 > /sys/devices/soc0/soc/2100000.aips-bus/2184000.usb/ci_hdrc.0/inputs/a_bus_req
I am following the procedure as per below
Linux/Documentation/usb/chipidea.txt - Linux Cross Reference - Free Electrons
The Board details : iMx6q sabre Auto infotainment board
Kernel Version : 4.1.15
Thanks and Regards
Shravan S
Hi Shravan S,
Sorry for late reply.
This is beyond my knowledge. I was expecting this to work out of the box.
It is clear that something is missing, but I do not know what. It might be worth doing some debugging in the USB driver. From what I could see, the code is located in drivers/usb/chipidea/. There is a "otg_fsm.c" file, it might worth checking that the OTG state machine is implemented correctly or is not blocked in some weird state.
Sorry but I can't help more.
regards
Gilles.