USB port is not detecting on i.MX6 Quad board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB port is not detecting on i.MX6 Quad board.

1,245 Views
rameshasp
Contributor IV


We are prototyping a custom board with the i.MX6 Quad processor part no is MCIMX6Q5EYM10AD and USB controller part is USB2422-I/MJ . We have 2 USB ports available, both ports are not detecting USB drive/Keyboard once boot the device.
Electrically i have probe and checked the voltage attached table below for reference.

(USB_PORT1)_USBPWR1  3.17V
(USB_PORT2)_USBPWR24.97V
ENA1.256V
ENB1.256V

Above table USB port is VCC is 3.17V which is not expected ENA(OCS1) 1.256V which is not expected.

Please help me to resolve this issue.

Advance Thanks,

Ramesha S P

Tags (1)
2 Replies

1,179 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ramesha

one can try to narrow down issue, checking if this is caused by USB2422 or i.MX6,

please check:

AN26.21 - USB Device Design Checklist

AN 26.2 - Implementation Guidelines for Microchip's USB 2.0 and USB 3.0 Hub Devices

i.MX6 usb side:

https://community.nxp.com/docs/DOC-105609 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,179 Views
rameshasp
Contributor IV

Thank you for your reply Igor,

My problem is while doing board bring up test if I connect any USB pendrive or keyboard it should detect, but in our it is not.

We are not able stop the u-boot and type any command .

Please help me to resolve this.

Advance Thank you,

Ramesha S P

0 Kudos
Reply