We are prototyping a custom board with the i.MX6 Quad processor part no is MCIMX6Q5EYM10AD and USB controller part is USB2422-I/MJ . We have 2 USB ports available, both ports are not detecting USB drive/Keyboard once boot the device.
Electrically i have probe and checked the voltage attached table below for reference.
| (USB_PORT1)_USBPWR1 | 3.17V |
| (USB_PORT2)_USBPWR2 | 4.97V |
| ENA | 1.256V |
| ENB | 1.256V |
Above table USB port is VCC is 3.17V which is not expected ENA(OCS1) 1.256V which is not expected.
Please help me to resolve this issue.
Advance Thanks,
Ramesha S P
Hi Ramesha
one can try to narrow down issue, checking if this is caused by USB2422 or i.MX6,
please check:
AN26.21 - USB Device Design Checklist
AN 26.2 - Implementation Guidelines for Microchip's USB 2.0 and USB 3.0 Hub Devices
i.MX6 usb side:
https://community.nxp.com/docs/DOC-105609
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you for your reply Igor,
My problem is while doing board bring up test if I connect any USB pendrive or keyboard it should detect, but in our it is not.
We are not able stop the u-boot and type any command .
Please help me to resolve this.
Advance Thank you,
Ramesha S P