USB mouse plug and play not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB mouse plug and play not working

934 Views
divyardharan
Contributor III

Hi

We are using imx 6 Q Sabre SDB board and we are using timestorm linux 3.0.

In our board the USB mouse plug and play functionality not working.

Scenario 1:

Once board is up,connect USB mouse to the port.

In the terminal it will show

usb 2-1: new low speed USB device number 2 using fsl-ehci

input: PixArt USB Optical Mouse as /devices/platform/fsl-ehci.1/usb2/2-1/2-1:1.0/input/input1

generic-usb 0003:0461:4E22.0001: input,hidraw0: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-fsl-ehci.1-1/input0.

But In the application it is not showing its mouse pointer.

Scenario 2 :

Connect the mouse.Start the board.

We can see mouse pointer in the application.

But my question is why mouse pointer is not showing when the board is already up??

Regards

Divya R Dharan

0 Kudos
Reply
0 Replies