USB midi gadget fails when connected to Mac (i.MX28 2.6.35)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB midi gadget fails when connected to Mac (i.MX28 2.6.35)

1,329 Views
LarsChristensen
Contributor I

Dear all,

We have a setup where we need a large block of data to be sent via midi to our target.

The midi gadget is being used and WIN7 see’s our target as a midi device. Our WIN7 application is capable of sending the large block of data without any problems.

If we connect our target to a MAC, the mac detects our target as a midi device, but our MAC application hangs, and the target outputs the following message:

udc: dTD error 00000060 QH=2

It should be mentioned that our WIN7 and MAC applications work with other midi products not running on a Linux platform.

We’ve tried several patches:

Peter Chan’s https://community.freescale.com/thread/314371

Disabling USB stream mode in the usbmode register.

Setting the FORCE_FULL_SPEED bit in the portsc1 register still hangs the MAC application at 0%, but the dTD error doesn’t happen.

Any help is appreciated

Regards,

Lars

Labels (2)
Tags (1)
0 Kudos
Reply
3 Replies

1,048 Views
YixingKong
Senior Contributor IV

Lars

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 Kudos
Reply

1,048 Views
YixingKong
Senior Contributor IV

Lars

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,
Yixing

0 Kudos
Reply

1,048 Views
fabio_estevam
NXP Employee
NXP Employee

Can you try this with kernel 3.12?

Regards,

Fabio Estevam

0 Kudos
Reply