USB location and display Chinese in imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB location and display Chinese in imx6

1,111 Views
shencheng
Contributor I

i want to load USB disk file in QT how can i know the location of the file? when i plug usb the location is change from /media/sda1 to /media/sda4 not s stable postion.

and if the file name is Chinese QT displayed it as question mark, how can i load Chinese named or any other not English named file in IMX6?

Labels (5)
0 Kudos
Reply
1 Reply

1,031 Views
igorpadykov
NXP Employee
NXP Employee

Hi shen

please check that usb disk was unmounted

How to mount and unmount usb drive or thumb drive in Linux | Linux basic configurations 

and locales configuration

i.MX6 Yocto Jethro release problem 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply