USB host control transfer data toggle problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB host control transfer data toggle problem

2,638 次查看
FredrikMoller
Contributor III

Background info: I'm writing a host controller driver for the i.MX28EVK.

Problem: When reading from device (i.e. the data phase of the control transfer is an IN transaction), host sends a DATA0 packet in the status phase. According to the USB 2.0 standard ch. 8.5.3, this should be a DATA1 packet. Is this a hardware issue? Is there any way to work around or solve the issue?

标签 (1)
0 项奖励
回复
1 回复

2,378 次查看
FredrikMoller
Contributor III

It was an error in my code. Hardware is fine. I relied on automatic data toggling which caused the controller hardware to toggle the data toggle from DATA1 (data phase) to DATA0 (status phase).

0 项奖励
回复