USB controller: Which field is the adress destination

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB controller: Which field is the adress destination

ソリューションへジャンプ
1,279件の閲覧回数
alexandredel
Contributor I

Hello

I'm working on the USB controller of the IMX 6Quad and i don't understand something. I read the documentation named "Application Processor Reference Manual", chapter 65, page 5270, but i don't find which field set up the adress destination for an iTD.

Is it the buffer pointer? Does someone knows this information? Or can help me to find it?

Thanks

Alexandre

ラベル(1)
0 件の賞賛
返信
1 解決策
1,189件の閲覧回数
Yuri
NXP Employee
NXP Employee

Yes, - the buffer pointer.

Note, new Reference Manual release (IMX6DQRM, Rev 2, 06/2014) is available now.

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,190件の閲覧回数
Yuri
NXP Employee
NXP Employee

Yes, - the buffer pointer.

Note, new Reference Manual release (IMX6DQRM, Rev 2, 06/2014) is available now.

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信