USB Wireless Wifi adapter and driver for iMX53 Ubuntu Linux on a Cortex-A8 processor

cancel
Showing results for 
Search instead for 
Did you mean: 

USB Wireless Wifi adapter and driver for iMX53 Ubuntu Linux on a Cortex-A8 processor

457 Views
RichardSideleau
Contributor I

I have a TRENDnet TEW654 wireless adapter connected to the RJ45 ethernet jack and is setup as an AP. I have the need for another NIC on the iMX53 board and am looking at a USB wireless adapter to be used as a client on another network with a different subnet. We had purchased an ASUS USB adapter that is compatible with Linux but there is no driver to this device for the Cortex-A8 processor. Is there a compatible USB wireless adapter and driver that will work on the Cortex-A8 processor? Thanks for any info.

Labels (1)
0 Kudos
0 Replies