USB Virtual RGB and IR camera on IMXRT1050

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Virtual RGB and IR camera on IMXRT1050

1,007 Views
Ismael_dz
Contributor II

Hello Community!!!

I want to create a USB video class device for a virtual RGB and IR camera on the IMXRT1050 dev board but Im a bit stuck in how to generate the endpoints for the USB protocol in order to recognize both devices.

Also I researched that I need to modify or create a BOS descriptor in order to have both the color and the sensor camera, but not exaclty sure how to add this part if Im using the example code in the SDK for a USB video virtual camera device.

0 Kudos
Reply
1 Reply

986 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @Ismael_dz ,

You should create a USB composite device for both RGB and IR camera. But there isn't such a demo. You can refer to the dev_composite_xxxx examples in SDK to see how to make a composite device, and AN12013 and it's software to see how to make a real UVC. You also can refer to SLN-VIZN3D-IOT sdk. It support UVC, switch between RGB/3D-IR/3D-depth. The sdk can be downloaded from https://mcuxpresso.nxp.com/.

 

Regards,

Jing

0 Kudos
Reply