Hi All,
Recently I downloaded Freescale Android 4.4.3 BSP Package and tested various interfaces with it in my sabresd board. While trying to test usb-otg interface using storage drives, I am able to mount the storage drives and view its contents but getting some log message,
init: no such service 'fuse_udisk'.
While comparing with the previous versions, I found that fuse_udisk service is missing in the init scripts and is not started anywhere.
Do I need to enable this service or just ignore this message?
Hi Lee,
I suggest you to complete the mount operation scripts in device/fsl/sabresd_6dq/init.rc like:
service fuse_sdcard /system/bin/sdcard -u 1023 -g 1023 -d /mnt/media_rw/sdcard /storage/sdcard
class late_start
disabled
Thanks.
Hi Haoran Wang,
Plat form IMX6SL
bluedroid on adroid kitkat 4.4.3
I have 2 issues one while data transfer, the other while enabling via GUI.
1) After enabling bluetooth, while transferring file from third party mobile to IMX_6SL board, file is getting transferred(TX), but vice versa (RX) is not happening, it is giving the error message :
File not Received
File : sample.jpg
Reason : Storage issue
2) And presently I am inserting my driver via GUI, I am getting an error message while enabling bluetooth via GUI ie Operation not permitted while loading .ko (driver)Please suggest me what to do?? whether I need to install my driver at boot by adding in init.rc?? if I do it always on boot bt will be in ON State only?? OR Do i need to build my driver along with android source code???
Please suggest me how to proceed further???
Thanks and Regards,
Mutyala Rao.