USB PHY stuck on iMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB PHY stuck on iMX6

1,287件の閲覧回数
sepsl
Contributor I

Hello!

We have a USB PHY stuck issue that occurs on the iMX6-Solo/DualLite and iMX6-Dual/Quad SoCs.

A 4-port hub is connected to the USB Host port on the SoC and on which the FTDI and TouchPanel devices are permanently connected. We use the third port for the GSM dongle.
At the moment when the Dongle connects to the network (at that time it has the highest current consumption) sometimes the USB PHY suddenly gets stuck - USB communication stops. After a problem occurs, the kernel tries to restart the subsystem but without success:

[ 3972.176598] usb 1-1.1-port3: cannot reset (err = -110)
[ 3973.197103] usb 1-1.1-port3: cannot reset (err = -110)
[ 3974.217184] usb 1-1.1-port3: cannot reset (err = -110)
[ 3975.236946] usb 1-1.1-port3: cannot reset (err = -110)
[ 3975.242097] usb 1-1.1-port3: Cannot enable. Maybe the USB cable is bad?
[ 3976.267275] usb 1-1.1-port3: cannot disable (err = -110)

You can only get out of this state by restarting the kernel driver "ci_hdrc_imx"

Has anyone encountered a similar issue or knows of any solution?

Thank you

Best regards

sepsl

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,263件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Is the USB hub self powered or not?
If the current drawn is to great maybe using a self powered hub may be a better idea.

Best regards/Saludos,
Aldo.

0 件の賞賛
返信

1,175件の閲覧回数
dousap2
Contributor I

The "-110" error typically occurs when the GSM dongle connects to a 2G 900 MHz network (2G 1800 MHz is not available in our country). In contrast, there are no issues when the dongle connects to a 4G network, although the exact frequencies used in those cases are unknown.

When the "-110" error arises, all devices connected to USB are completely stuck. Although the connected device is still detected by Linux (e.g., through the lsusb command), any communication with any USB-connected device fails completely—no data transfer occurs. This state persists for at least 5 minutes without recovering automatically.

The issue occurs regardless of whether USB communication is in full-speed or high-speed modes. However, in full-speed mode, the frequency of USB hangs is reduced. These registers are used to enable Full-speed:
PFSC in USB_nPORTSC1
RXPWDDIFF and RXPWDENV in USBPHYx_PWDn.

The GSM dongle has its own power supply with a 2A current limit. Despite this high limit, power drops are observed due to the dongle's peak consumption during communication. Other power supplies in the system, including the USB hub, remain stable. Interestingly, these power drops occur even when the dongle is connected to a PC, where communication remains stable.

We tested a USB hub with its own power supply, but the USB hang still occurred. In another experiment, connecting multiple unpowered USB hubs in series resolved the issue only after the 3rd hub (4 hubs total) was added. Additionally, when using an optical USB splitter (with its own power supply) to place the dongle 4 meters away from the device, the USB hang did not occur. However, when the dongle was placed closer to the device, the issue reappeared. These observations suggest that GSM 2G 900 MHz communication interference affects USB communication, whether the interference occurs over the air or via the USB cable.

During debugging, we found that the following register statuses were sometimes (though not always) set when the issue occurred:
UTMI_RXERROR_FAIL_COUNT in the USBPHYx_DEBUG0_STATUS register
UEI in the USB_nUSBSTS register

To restore communication from a stuck state, it will help to reinitialize the USB-PHY peripheral (set the SFTRST bit in the USBPHYx_CTRLn register and then complete the USB-PHY initialization) and also send a reset using the Single-ended zero state (in Linux using USB_REQ_SET_FEATURE with USB_PORT_FEAT_RESET).

We also observed that an external trigger, such as a Single-ended one state lasting more than 1.125 µs (generated using an external signal generator), can lead to a complete USB hang. While the hang does not occur immediately, it manifests after several Start-of-Frame (SOF) packets. The consequences of this issue are identical to those observed with the GSM dongle, but we are not certain if the root cause is the same.

 

5V input voltage before the dongle power supply in communication with AP:

scope_6.png

 

A closer look at the 5V input voltage before the dongle power supply in communication with AP (Green - 5V power supply, yellow - current from dongle):

scope_15.png

 

Voltage measured on the dongle with PC:

scope_11.png

 

USB stuck at full speed with USB dongl (I don't know what signal appeared after 133 us):

Snímek obrazovky_20241119_192156.png

 

Injection Single-ended one 1.125 µs:

Snímek obrazovky_20241120_141101.png

 

A closer look at the injection Single-ended one:

Snímek obrazovky_20241120_141244.png

 

High-speed levels after USB stuck. Green and yellow D+ and D- USB:

Snímek obrazovky_20241121_163822.png

 

Measurement of interference with USB dongle (yellow - USB communication, green - open input, red - measurement GND with probe) (the interference voltage level may not correspond to reality, the probe was not adapted to measure such high frequencies):

Snímek obrazovky_20241121_163348.png

0 件の賞賛
返信