USB OTG ID Pin on i.MX7Sabre

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB OTG ID Pin on i.MX7Sabre

300 Views
marcfigliuolo
Contributor I

Thank you for the information. Then I will pull the ID high for Device use.

I think my first question was not formulated very good. So a 2nd try:

OTG2 on the Evalboard is used as Host only, its done with a 4 Pin USB Plug. OTG specification says if you use an OTG interface as host, you have to pull the ID pin with resistance < 10 Ohms to GND.

But in the Evalboard its pulled down with 10 kOhms. Is the function garanteed if you do it like this?

10k Ohms >>10 Ohms which is specified by the standard.

0 Kudos
0 Replies