USB_OTG_HOST_MODE pin not described in reference manual

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB_OTG_HOST_MODE pin not described in reference manual

891件の閲覧回数
emil
Contributor III

Hello,

What is the function of the USB_OTG_HOST_MODE pin on the iMX6Solo?I get the feeling that you want to set this pin if you use the OTG interface only as host, but what do I set it to? And what is the exact purpose and function?

BR,

Emil

ラベル(3)
0 件の賞賛
4 返答(返信)

638件の閲覧回数
Yuri
NXP Employee
NXP Employee

The USB_OTG_HOST_MODE can be used for indicating the USB OTG core is working in Host mode.

USB_OTG_HOST_MODE = 0 indicates the USB is operating in Device mode

USB_OTG_HOST_MODE = 1 indicates the USB is operating in Host mode


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

638件の閲覧回数
tomo
Contributor II

Hello,

This signal is output, isn't it?

Best regards,

Tomo

0 件の賞賛

638件の閲覧回数
Yuri
NXP Employee
NXP Employee

Yes, the signal is output.


Regards,

Yuri.

0 件の賞賛

638件の閲覧回数
tomo
Contributor II

Thank you for your reply.

Best Regards,

Tomo

0 件の賞賛