USB Camera in JB 4.2.2-1.0.0 SabreSD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Camera in JB 4.2.2-1.0.0 SabreSD

ソリューションへジャンプ
6,209件の閲覧回数
Chris1z
Contributor III

I've enabled the USB camera on JB 4.2.2 SabreSD board using the following patch.  When I test it with a Logitech Webcam C250 and the "Camera" app, I see a lot of video glitches.  Pointing it at a static location, I see glitches every 5-10 seconds.  And if I wave my hand in front of the camera the video glitches are worse.

Is there a way to improve the USB video decoding performance?

diff --git a/sabresd_6dq/BoardConfig.mk b/sabresd_6dq/BoardConfig.mk

index 8ecf4a7..ef53f05 100755

--- a/sabresd_6dq/BoardConfig.mk

+++ b/sabresd_6dq/BoardConfig.mk

@@ -97,6 +97,8 @@ USE_GPU_ALLOCATOR := true

# camera hal v2

IMX_CAMERA_HAL_V2 := true

+BOARD_HAVE_USB_CAMERA := true

+

# define frame buffer count

NUM_FRAMEBUFFER_SURFACE_BUFFERS := 3

diff --git a/sabresd_6dq/init.rc b/sabresd_6dq/init.rc

index 4420c07..70f7cae 100755

--- a/sabresd_6dq/init.rc

+++ b/sabresd_6dq/init.rc

@@ -52,10 +52,10 @@ on boot

     #For landscape mode, orient is 0

     #For portrait mode, orient is 90

     #the android before honycomb are all in portrait mode

-    setprop back_camera_name ov5640_mipi

+    setprop back_camera_name uvc

     setprop back_camera_orient 0

-    setprop front_camera_name uvc,ov5642_camera,ov5640_camera

-    setprop front_camera_orient 0

+    #setprop front_camera_name uvc

+    #setprop front_camera_orient 0

     # Set OpenGLES version

     setprop ro.opengles.version 131072

ラベル(3)
タグ(5)
0 件の賞賛
返信
1 解決策
4,143件の閲覧回数
Ivan_liu
NXP Employee
NXP Employee

Hi Chris1z,

The usb camera is not a "bad" camera. It is ok when connected to PC.

It should be some other module like WIFI with high frequency impact the usb bus receiving data from usb camera.

Or, it may be usb camera does not have good anti-jamming to high frequency.

BRs,

Xiaowen

元の投稿で解決策を見る

0 件の賞賛
返信
13 返答(返信)
4,143件の閲覧回数
Chris1z
Contributor III

Thank you Karina, but this was not my issue.  I can connect the UVC camera just fine and see video.  I am more concerned with the video performance and video glitches we see when using the camera.

0 件の賞賛
返信
4,143件の閲覧回数
Ivan_liu
NXP Employee
NXP Employee

hi, it should be eletromagnetic compatibility issue.

please take another usb camera to have a try.

0 件の賞賛
返信
4,143件の閲覧回数
Chris1z
Contributor III

Thanks for your replay Xiaowen.  I've tried 3 other cameras with the same issue:

Creative Live Cam VF0690

Microsoft LifeCam Cinema

Our custom USB camera

0 件の賞賛
返信
4,143件の閲覧回数
Ivan_liu
NXP Employee
NXP Employee

hi Chris1z

please refer to our Release Note to chose the usb camera supported in our platform.


Media - USB Camera

Y

Y

Y

Logitech:

  • C250
  • E3500

The usb camera you used to do test is not supported in our platform.

0 件の賞賛
返信
4,143件の閲覧回数
9crkzhou
Contributor III

where is this Relese Note ?

can you give me a link? or a full name

0 件の賞賛
返信
4,143件の閲覧回数
Chris1z
Contributor III

The release notes document is Android_Release_Notes.pdf.  It's found in the "docs" directory of the jb4.2.2-1.1.0-ga Android release.

0 件の賞賛
返信
4,143件の閲覧回数
Chris1z
Contributor III

Hi Xiaowen,

Please read my original post.  I tested it with C250.  I only mentioned the other cameras when you suggested trying other cams.

Chris

0 件の賞賛
返信
4,143件の閲覧回数
Ivan_liu
NXP Employee
NXP Employee

hi Chris1z,

what I mean that please try other usb cameras that suppported.

Even the same kind usb cameras may have different electromagnetic response.

please ignore the usb cameras that not supported.

Xiaowen

0 件の賞賛
返信
4,143件の閲覧回数
Chris1z
Contributor III

Xiaowen,

I only have access to one C250.  I'm not sure I understand how this could be an EMI issue.  It seems more like a video decoding issue.  Can you elaborate more on what the electromagnetic issue would be? Would other USB devices on the bus have this problem? Is there something we can probe?

Thanks,

Chris

0 件の賞賛
返信
4,143件の閲覧回数
Ivan_liu
NXP Employee
NXP Employee

hi Chris1z,

Because we have met the similar problem when do preview.

It is ok after we replaced it with another usb camera.

So, can you make sure that it is ok when do preview.

Does the issue only happen with recording.

When do recording, it also do preview.

So, the issue you mentioned happens on preview output or the encoded video file when do recording. 

BRs,

Xiaowen

0 件の賞賛
返信
4,143件の閲覧回数
Chris1z
Contributor III

Xiaowen,

We would see this issue on the preview and remote side of a Skype call.  I'm still trying to understand the EMI issue...we have 4 different camera vendors that exhibit this problem?  Is the issue on the USB bus or are you saying the actual cameras are faulty?  Would it happen to the "bad" camera if it was hooked up to a PC?

Thanks,

Chris

0 件の賞賛
返信
4,144件の閲覧回数
Ivan_liu
NXP Employee
NXP Employee

Hi Chris1z,

The usb camera is not a "bad" camera. It is ok when connected to PC.

It should be some other module like WIFI with high frequency impact the usb bus receiving data from usb camera.

Or, it may be usb camera does not have good anti-jamming to high frequency.

BRs,

Xiaowen

0 件の賞賛
返信