USB 3.0 voltage swing tunning

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB 3.0 voltage swing tunning

Jump to solution
1,425 Views
pavel_drabek
Contributor I

How I can tune voltage swing to pass USB 3.0 compliance?

I am getting only: PeakToPeakVoltage (5G) (Short Channel) [32241] 63.3 mV, while Pass Limits: [100.0 mV to 1.2000 V]

Thank you.

Best regards

Pavel

0 Kudos
1 Solution
1,319 Views
pavel_drabek
Contributor I

OK, got it, this is the magic:

1) Boot linux

2) memtool 0x5b198004=0x3f

3) memtool 0x5b198030=0x03

4) Plug USB fixture and conduct measurements

View solution in original post

0 Kudos
2 Replies
1,320 Views
pavel_drabek
Contributor I

OK, got it, this is the magic:

1) Boot linux

2) memtool 0x5b198004=0x3f

3) memtool 0x5b198030=0x03

4) Plug USB fixture and conduct measurements

0 Kudos
712 Views
giuseppepagano1
Contributor III

Hi Pavel,

thank you for sharing your solution. We are facing the same issue on our custom board based on imx8QM.

 

Can I ask you where did you find this information or USB3.0 PHY register map?

Thank you in advance.

 

Best Regards

Giuseppe Pagano 

Tags (1)
0 Kudos