USB 3.0 not working on iMX6QP based custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB 3.0 not working on iMX6QP based custom board

1,175 Views
kishorr
Contributor II

We are working on a iMX6QP based custom board where USB3.0 Controller (USBT7320) is connected to PCIE.

The USB controller is getting listed with lspci command. Also after enabling xHCI driver, two usb 3.0 root hubs are also seen with lsusb command.

Following is the error when I plug in usb device into usb 3.0 ports---

root~# usb 3-2: device no response, device descriptor read/64, error -71
xhci_hcd 0000:01:00.0: Setup ERROR: setup context command for slot 1.
usb 3-2: device no response, device descriptor read/64, error -71
xhci_hcd 0000:01:00.0: Setup ERROR: setup context command for slot 1.
usb 3-2: device not accepting address 4, error -71
usb 3-2: device not accepting address 5, error -71
hub 3-0:1.0: unable to enumerate USB device on port 2

To isolate the issue we have used TI USB 7320 EVM and connected it to Sabre Ref board.

With this setup the USB 3.0 ports are working.

The only difference I see is Sabre Ref board has iMX6Q and the custom board has iMX6QP.

Not sure if there is any issue in using the iMX6QP-PCIE interface when plugged with USB3.0 controller.

Any comments on this issue are appreciated.

Thanks

Kishor

Tags (2)
0 Kudos
Reply
1 Reply

918 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kishor

below some specifc for i.MX6QP patches, one can try them

https://lists.denx.de/pipermail/u-boot/2015-October/229543.html 

linux-2.6-imx.git - Freescale i.MX Linux Tree 

had you tried latest bsps from

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply